What are you looking for?
Suggested searches
No product matches found - System Exception
Matched content
HP DeskJet 940C printer driver for E5071A
This printer driver is only used for the E5071A with the following serial numbers and for using the HP DeskJet 940C with the E5071A. This driver is not required if the software has already been installed into the E5071A.
E5071A JP1KJ00100 through 248,251,253.
Required E5071A Firmware Revision
Rev.A.01.00 and above
Installation Procedure
Step1. Prepare five floppy disks.
Step2. Label disk with disk number (e.g. disk1, disk2, .. disk5).
Step3. Insert the floppy disk labeled "disk1" into your computer's FDD.
Step3. Click on the "Printer driver [disk1]" listed below.
Step4. Copy the file onto the disk.
Step5. Repeat each file onto each disk.
Keysight recommends using the most current version, which includes the most up-to-date bug fixes and security patches available.
Release Date | Version | Version Description |
---|---|---|
2002-08-19 | n/a | Printer driver [disk1] |
Release Date | Version |
---|---|
2002-08-19 | n/a |
Version Description |
---|
Printer driver [disk1] |
How to Download
- Download all of files.
How to Install
- See Above
Licensing
- Does Not Require a License
Add-On Software / Utilities
Downloads
Installs on: PC
Operating System
- Windows XP
Prerequisites
- See Above
Supported Instruments
- E5070A E5071A
No previous versions available
SHOW MORE