What are you looking for?
Suggested searches
No product matches found - System Exception
Matched content
HP DeskJet 940C printer driver for E5071A
This printer driver is only used for the E5071A with the following serial numbers and for using the HP DeskJet 940C with the E5071A. This driver is not required if the software has already been installed into the E5071A.
E5071A JP1KJ00100 through 248,251,253.
Required E5071A Firmware Revision
Rev.A.01.00 and above
Installation Procedure
Step1. Prepare five floppy disks.
Step2. Label disk with disk number (e.g. disk1, disk2, .. disk5).
Step3. Insert the floppy disk labeled "disk1" into your computer's FDD.
Step3. Click on the "Printer driver [disk1]" listed below.
Step4. Copy the file onto the disk.
Step5. Repeat each file onto each disk.
是德建议使用最新的版本,其中包括最新的漏洞修复和安全补丁
发布日期 | 版本 | 版本说明 |
---|---|---|
2002-08-19 | n/a | Printer driver [disk1] |
发布日期 | 版本 |
---|---|
2002-08-19 | n/a |
Version Description |
---|
Printer driver [disk1] |
如何下载
- Download all of files.
如何安装
- See Above
颁发许可证
- Does Not Require a License
附加的软件/实用程序
下载
Installs on: PC
操作系统
- Windows XP
前提要求
- See Above
支持的仪器
- E5070A E5071A
没有可用的软件版本
SHOW MORE