Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

N1996A CSA Spectrum Analyzer Firmware Update

Keysight CSA Spectrum Analyzer

Updating the firmware in your spectrum analyzer has never been easier!!

  1. Download the USB .zip update file below to a local PC drive
  2. Extract the downloaded .zip file to a USB storage device
  3. Insert the USB device into one of the 3 instrument USB ports
  4. Turn the instrument on and follow the simple on-screen prompts

Please Note:

  • While the files contained in the PCMCIA update version can also be used when installing the firmware via USB, it is intended for use by a qualified service technician. The only difference between the two versions is that the PCMCIA version also contains a few extra files required to boot the instrument from the internal PCMCIA slot if needed during servicing the instrument.

WARNING:

  • Do not attempt to use this update on an instrument that is currently using a Beta version of firmware without first contacting the Keysight representative responsible for the instrument for further required instructions. Failing to do so could render the instrument unusable.

To receive automatic email notifications on such things as new firmware released sign up for Keysight Email Updates

No previous versions available.