Keysight CSA Spectrum Analyzer

Updating the firmware in your spectrum analyzer has never been easier!!

  1. Download the USB .zip update file below to a local PC drive
  2. Extract the downloaded .zip file to a USB storage device
  3. Insert the USB device into one of the 3 instrument USB ports
  4. Turn the instrument on and follow the simple on-screen prompts

Please Note:

  • While the files contained in the PCMCIA update version can also be used when installing the firmware via USB, it is intended for use by a qualified service technician. The only difference between the two versions is that the PCMCIA version also contains a few extra files required to boot the instrument from the internal PCMCIA slot if needed during servicing the instrument.

WARNING:

  • Do not attempt to use this update on an instrument that is currently using a Beta version of firmware without first contacting the Keysight representative responsible for the instrument for further required instructions. Failing to do so could render the instrument unusable.

To receive automatic email notifications on such things as new firmware released sign up for Keysight Email Updates

是德建议使用最新的版本,其中包括最新的漏洞修复和安全补丁
发布日期 版本 版本说明
2010-06-16 A.02.07 22 M Downloadable .zip file.
发布日期 版本
2010-06-16 A.02.07
Version Description
22 M Downloadable .zip file.

如何下载

  • See Documentation

如何安装

  • See Documentation

颁发许可证

  • Does Not Require a License

Installs on: Instrument

前提要求

  • See Documentation

支持的仪器

  • N1996A
没有可用的软件版本
SHOW MORE