이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

P-Series Power Meter Firmware Upgrade

Applicable for N1911A and N1912A power meters.

Compatibility: P-Series N1911A and N1912A power meters.

Please note that after the firmware is installed into the power meter an additional digit will be added to the firmware revision. The number added after the first letter in the firmware revision will designate the number of power sensor channels in the power meter. For example the A.05.04 firmware installed in a two channel N1912A will now be shown as A2.05.04 on the display of the power meter; installed in a one channel N1911A the firmware revision will be A1.05.04.

NOTE: Power meter with the serial number MY58410000 and above, SG58410000 and above will only support firmware version of A.06.01 and above.

릴리스 날짜 버젼 버전 설명
2018-12-07 A.06.01 P-Series Firmware A.06.01.exe

다운로드 방법

  • Please refer to P-Series Power Meter Firmware Upgrade Procedure.

설치 방법

  • Please refer to P-Series Power Meter Firmware Upgrade Procedure.

라이센스

  • 라이센스 필요 없음

지원 문서

부가 소프트웨어 / 유틸리티

다운로드

설치 위치:

Instrument

사전 조건

  • Please refer to P-Series Power Meter Firmware Upgrade Procedure.

지원되는 계측기

  • N1911A, N1912A