이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

E5805A USB/4-port RS232 PC Driver

Install the correct file below based on your operating system, either Windows® 2000/XP or Windows 98. By running one of these .exe files you will be saving them to a directory on your system. Then, when you plug in the E5805A to your USB port it will prompt you for the location of the files.

Windows is a U.S. registered trademark of Microsoft Corporation.

릴리스 날짜 버젼 버전 설명
2005-05-26 v2.88 Load the file here and save to the suggested folder. Once the E5805A is plugged in it will prompt you to point to the directory that you saved these files too.

다운로드 방법

  • See Above

설치 방법

  • 사용 가능한 정보 없음

라이센스

  • 라이센스 필요 없음