这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

E5805A USB/4-port RS232 PC Driver

Install the correct file below based on your operating system, either Windows® 2000/XP or Windows 98. By running one of these .exe files you will be saving them to a directory on your system. Then, when you plug in the E5805A to your USB port it will prompt you for the location of the files.

Windows is a U.S. registered trademark of Microsoft Corporation.

发布日期 版本 版本说明
2005-05-26 v2.88 Load the file here and save to the suggested folder. Once the E5805A is plugged in it will prompt you to point to the directory that you saved these files too.

如何下载

  • See Above

如何安装

  • 无此信息

颁发许可证

  • 不要求具有许可证