Here’s the page we think you wanted. See search results instead:

 

Discutez avec un expert

E5805A USB/4-port RS232 PC Driver

Install the correct file below based on your operating system, either Windows® 2000/XP or Windows 98. By running one of these .exe files you will be saving them to a directory on your system. Then, when you plug in the E5805A to your USB port it will prompt you for the location of the files.

Windows is a U.S. registered trademark of Microsoft Corporation.

Release Date Version Version Description
2005-05-26 v2.88 Load the file here and save to the suggested folder. Once the E5805A is plugged in it will prompt you to point to the directory that you saved these files too.

How to Download

  • See Above

How to Install

  • Information Not Available

Licensing

  • Does Not Require a License
Download

Installs on:

PC

Operating System

  • Windows XP
  • Windows 2000

Prerequisites

  • Information Not Available

Supported Instruments

  • E5805A

Related Links