您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

E5805A USB/4-port RS232 PC Driver

Install the correct file below based on your operating system, either Windows® 2000/XP or Windows 98. By running one of these .exe files you will be saving them to a directory on your system. Then, when you plug in the E5805A to your USB port it will prompt you for the location of the files.

Windows is a U.S. registered trademark of Microsoft Corporation.

發佈日期 版本 版本說明
2005-05-26 v2.88 Load the file here and save to the suggested folder. Once the E5805A is plugged in it will prompt you to point to the directory that you saved these files too.

如何下載

  • See Above

如何安裝

  • 無相關資訊

授權

  • 不需要授權