The following options must be installed in an N4010A instrument to support this software:

  • Option 102 or Option 103 (WLAN Measurement Capability)
  • Option 104 (Fully Flexible ARB)
  • Option 204 (Signal Studio License)
Keysight recommends using the most current version, which includes the most up-to-date bug fixes and security patches available.
Release Date Version Version Description
2005-10-06 A.02.09 Added control of the sample rate to the main screen. Removed the Export feature from the File menu in order to prevent confusion.
Release Date Version
2005-10-06 A.02.09
Version Description
Added control of the sample rate to the main screen. Removed the Export feature from the File menu in order to prevent confusion.

How to Download

  • Click the Download button. Select the appropriate executable file. Choose Run.

Licensing

  • Does Not Require a License

Installs on: PC

Prerequisites

  • See Above

Supported Instruments

  • N4010A
No previous versions available
SHOW MORE