这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

Firmware Update for B2200A/B2201A

Instrument Installation:
This firmware is installable into the following instruments.

  • B2200A
  • B2201A

Firmware Revision:
A.01.04

Resolved Issues:

The following defects are fixed.
- B220x doesn't turn on LED if touched
- Firmware is aborted when a ":rout:func dcon" command is received
- B2200A switching takes approximately 1 second in worst case if LED is ON

没有先前版本。