Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

3070 05.32pa Software Package

3070 05.32pa Software Package Release Notes and Download

3070 05.32pa corrects an installation problem found in 3070 05.32p. 3070 05.32p would remove files from the etc, util, diagnostics, and qm directories on some computers. The new 3070 05.32pa software does not remove any files, and it will replace the missing files on computers that were damaged by installation of 3070 05.32p.

3070 05.32pa is in the form of two Software Updates and a Documentation Update:

  • The first Software Update contains only the Keysight 3070 05.32pa software. It is for customers who do not use the ASSET InterTech ScanWorks boundary-scan product. This Software Update is 83 MB.
  • The second Software Update contains the Keysight 3070 05.32pa software and ASSET InterTech ScanWorks version 3.4 This Software Update is 303 MB.

Both Software Updates are much bigger than most previous 3070 software patches, but they are not a complete 3070 installation. In order to get the size down we eliminated many files that did not change between 05.30, and 05.32, such as Keysight Digital Libraries, 3070 Online Help files, MKS Toolkit, and Java runtime environment. This is similar to the form of the 05.31p Software Update.

These Software Updates may be installed only on MS Windows systems with 3070 05.30p or 05.31p (or any patch level of these versions, e.g. 05.30pc, 05.31pa). They can be installed on systems with 3070 Test System Software or 3070 Development Software. The Software Update will replace most of the 3070 05.30 programs with 3070 05.32 programs.

The Software Update must be installed by the administrator login (or a login with administrator privileges).

The documentation update may be installed on MS Windows systems. It can be installed with Keysight 3070 application software, or by it's self. The User Manuals for currently supported 3070 products are being delivered in a new format with this release. This new HTML format provides a reorganization of the material and better search capabilities. To learn about the features of the on-line documentation, download and install the documentation update and then open the on-line documentation using the desktop icon or Start>Programs>Keysight 3070>On-Line Manuals>3070 05.32 On-Line Documentation. Once you are in the on-line documentation, navigate to Getting Started>Getting Started>The Keysight 3070 On-Line Documentation.

To download the 05.32pa Software Update without ScanWorks on Windows systems running the 3070 05.30p, or 05.31p software release:

  1. Click on 3070 05.32pa 0804 WN Download. Save this file to disk.
  2. Close all open programs.
  3. Go to the directory in which the file was saved and double-click on Agilent3070_0532pa.exe.
  4. Follow the Install Shield instructions for installation.
  5. To validate that the software installed correctly, bring up a Korn Shell window. On the menu bar, click START then click Programs then click Agilent3070 then click Korn Shell. In the Korn Shell window, type version and return. The software revision "3070 05.32pa 0804 WN" should display.
  6. Delete the Agilent3070_0532pa.exe file.

To download the 3070 05.32pa Software Update that includes ScanWorks 3.4 on Windows systems running the 3070 05.30p, or 05.31p software release:

  1. Go to Control Panel\Add Remove Programs.
  2. Select ScanWorks 3.3.1. Click on Change\Remove.
  3. Click on Next in the InstallShield Wizard to uninstall ScanWorks.
  4. Click on 3070 05.32pa 0804 WN with ScanWorks 3.4 Download. Save this file to disk. You will need 650MB of free space to download this file and extract the installation files.
  5. Close all open programs.
  6. Go to the directory in which the file was saved and double-click on Agilent3070_0532pa_withScanWorks.exe.
  7. The WinZip Self-Extractor will ask you where to extract the installation file. The default location is c:\3070Update. Make sure that you have at least 317MB of space available to extract the installation files.
  8. Click on Unzip. When the extraction is complete you get a message box that says "263 file(s) unzipped successfully" Click on OK. Then click on Close in the WinZip Self-Extractor form.
  9. Delete the file Agilent3070_0532pa_withScanWorks.exe.
  10. Go to the directory where you extracted the installation files. Double click on setup.exe.
  11. Follow the Install Shield instructions for installation.
  12. To validate that the software installed correctly, bring up a Korn Shell window. On the menu bar, click START then click Programs then click Agilent3070 then click Korn Shell. In the Korn Shell window, type version and return. The software revision "3070 05.32pa 0804 WN" should display.
  13. Delete the directory where you extracted the installation files.

To download the documentation update on Windows systems:

  1. Click on 3070 05.32p Documentation Update for Windows. Save this file to disk.
  2. Close all open programs.
  3. Go to the directory in which the file was saved and double-click on Agilent3070_05.32_OnlineDocs.exe.
  4. Follow the Install Shield instructions for installation.
Дата выпуска Версия Описание версии
2004-11-12 05.32pa 3070 05.32pa 0804 WN Download

Как загрузить

  • See Above

Как установить

  • See Above

Лицензии

  • Лицензия не требуется

Сопроводительная документация

Загрузить

Устанавливается на:

PC

Предварительные условия

  • See Above

Поддерживаемые приборы

  • i3070