Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discuter avec un expert

33502A Firmware Update

Date de mise en circulation Version Description de la version
2020-03-18 2.02 Update to resolve memory leak

Comment télécharger

  1. Click the Download button.
  2. Save the firmware file to your computer and note the directory where the file is saved.
  3. Unzip the file to access the .upd file. For updates using the front panel USB drive, the utility extracts the required files from the unzipped .upd file.
  4. If not currently installed, download and install the Firmware Update Utility.

Comment installer

  1. From the Start menu, start the Firmware Update Utility (FWUpdate.exe). The utility will prompt you for the location of the .upd file. Follow the additional prompts to complete the installation.
  2. If updating from the LAN, USB interface, the instrument address is required. With the instrument turned on, pressing Help-About displays the addresses.
  3. The update may take several seconds to complete and will reboot the instrument. After the update is complete, exit the utility.
  4. It is not necessary to re-calibrate the instrument following a firmware update. 

Autorisation d'exploitation

  • Ne requiert aucune licence

Document d'appui

Logiciels additionels/utilités

Téléchargez

S'installe sur:

Instrument

Système d'exploitation

  • Windows 7
  • Windows Vista
  • Windows XP
  • Windows 10

Préalables

  • Information non-disponible

Instruments appuyés

  • 33502A