What are you looking for?
N19306B PLTS PAM4 Eye Diagram
The new N19306B Physical Layer Test System (PLTS) 2024 has significant breakthrough capabilities with regards to resolving adjacent impedance discontinuities within high-speed interconnects, such as cables, backplanes, PCBs and connectors. Many signal integrity laboratories around the world have benefited from the power of PLTS in the R&D prototype test phase. PLTS N19306B extends the N19301B base product to perform PAM4 eye diagram analysis beyond the default NRZ eye diagram analysis in the base N19301B
Release Date | Version | Version Description |
---|---|---|
2024-01-19 | 2024 | See Supporting Documentation for details |
Release Date | Version |
---|---|
2024-01-19 | 2024 |
Version Description |
---|
See Supporting Documentation for details |
How to Download
Click on “Download” button indicated on Keysight website
How to Install
- When Install wizard launches, just click install and make sure to use all standard default settings (no custom settings should be used).
- After installation, the first time PLTS launches, it will ask for the license file. Just browse to your location that you saved the license file to and double click on license file.
- The program will then automatically start working properly. Sample s-parameter data files can be found under install folder labeled “Data” that is by standard default located here: This PC OSDisk (C:) > Program Files > Keysight > PLTS2024 > Data
Licensing
- Requires a License
N19301B trial will enable all features N19303B/5B/6B/7B/8B
Supporting Documentation
Installs on: PC / Instrument
Operating System
- Windows 10
- Windows 11
Prerequisites
- Information Not Available
Supported Instruments
- ENA/PNA/PNA-X/PXI-VNA/USB-VNA/TDR
How to Download
Click on “Download” button indicated on Keysight website
How to Install
- When Install wizard launches, just click install and make sure to use all standard default settings (no custom settings should be used).
- After installation, the first time PLTS launches, it will ask for the license file. Just browse to your location that you saved the license file to and double click on license file.
- The program will then automatically start working properly. Sample s-parameter data files can be found under install folder labeled “Data” that is by standard default located here: This PC OSDisk (C:) > Program Files > Keysight > PLTS2021 > Data
Licensing
- Requires a License
N19301B trial will enable all features N19303B/5B/6B/7B
Supporting Documentation
Installs on: PC / Instrument
Operating System
- Windows 8
- Windows 7
Prerequisites
- Information Not Available
Supported Instruments
- Keysight VNA/ENA/TDR
How to Download
Click on “Download” button indicated on Keysight website
How to Install
- When Install wizard launches, just click install and make sure to use all standard default settings (no custom settings should be used).
- After installation, the first time PLTS launches, it will ask for the license file. Just browse to your location that you saved the license file to and double click on license file.
- The program will then automatically start working properly. Sample s-parameter data files can be found under install folder labeled “Data” that is by standard default located here: This PC OSDisk (C:) > Program Files > Keysight > PLTS2020 > Data
Licensing
- Requires a License
Supporting Documentation
Installs on: PC / Instrument
Operating System
- Windows 8
- Windows 7
Prerequisites
- Information Not Available
Supported Instruments
- Keysight VNA/ENA/TDR