This is an example program that works with the following Model Numbers:
• N8937APV
• N8957APV

This example program demonstrates how to program the N8900APV units in fixed mode. It demonstrates how to set the output, set the output protection, and how to perform measurements. Source files are included for VB.NET using Keysight VISA-COM, C# using VISA-COM, Python3 using PyVisa, and also a plain text file. The plain text file includes all of the instrument commands and some comments. These programs are free to modify.

キーサイトは、最新のバグ修正とセキュリティパッチを含む、利用可能な最新バージョンを使用することをお勧めします。
リリース バージョン 内容
2019-08-12 A.00.00 Keysight N8937APV and N8957APV PhotoVoltaic Simulator Output Programming Example
リリース バージョン
2019-08-12 A.00.00
Version Description
Keysight N8937APV and N8957APV PhotoVoltaic Simulator Output Programming Example

Included Files:
VB.NET using Keysight VISA-COM
C# using VISA-COM
Python 3 using PyVisa
Plain text file
Note: Keysight VISA-COM requires that the Keysight IO Libraries are installed.

ダウンロード方法

  • Download source file and use with your preferred programming environment

インストール方法

  • Information Not Available

ライセンス

  • Does Not Require a License

Installs on: PC

OS

  • Any

前提知識

  • Information Not Available

対象測定器

  • N8937APV, N8957APV
ソフトウェアバージョンはご利用いただけません
SHOW MORE