Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

KS83200A Automation Software for Automotive Radar – Basic

KS83200A compliments the E8740A automotive radar solutions. Enabling features and test sequences for both transmit and receiver testing. Simply instrument connection, correction and calibration for E8740A hardware configurations 010-090.

Дата выпуска Версия Описание версии

Имеется бесплатная демо-версия

2019-06-03 1.0 Initial release for automation, connection, correction of automotive radar test setups.

Как загрузить

  • Click Download button on this page to download the KS83200A Automation software. This software is a plugin to the Test Automation PathWave (TAP)
    Note: Receiver testing and ETSI test cases can also be added with KS83RX0A and KS83ST0A respectively

Как установить

  • The SW components required are installed separately. Please install the components in the following order:
    1. Please ensure you have the TAP Development system application installed. version 8.8. KS8400A
    2. To automate any of the receiver tests you will also need Signal Studio software suite version 1.2.0.0. N7608APPC
    3. To see the results on an oscilloscope you will need to have VSA software. 89600A VSA software
    4. KS83200A automotive radar plugins

Лицензии

Сопроводительная документация

Загрузить

Устанавливается на:

PC / Instrument

Операционная система

  • Windows 7 Service pack 1 (32/64-bit)
  • Windows 10 (32/64 bit)

Предварительные условия

  1. TAP Development System application KS8400A version 8.8 or later (this will also install the Keysight license manager)
  2. Signal Studio software suite N7608APPC version 1.2.0.0 or later (refer to the user guide for more information and a particular hardware configuration)
  3. 89600A VSA software version 2019.0301 or later (refer to the user guide for more information and a hardware configuration)
  4. M8195A Firmware and Soft front panel version 3.6 or later (this is used for signal general or receiver testing - (refer to the user guide for more information and a each hardware configuration)
     

Поддерживаемые приборы

  • KS83200A Software can be installed onto the spectrum analyzers •N9041B or N9040B.

Ссылки, относящиеся к этой теме