您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

E7760B "Wideband Transceiver Instrument Software"

Learn more about the 5G Non-signaling mmWave Test Solution measurement application

This process will update the instrument software and all the measurement applications.  Measurement applications require a license key to enable their functionality. 

Installing the latest instrument software version is encouraged to guarantee that your E7760B instrument compatibility and performance.

Keysight always recommends using the most current version of the instrument software.  New releases of instrument software keeps your instrument up to date with features, enhancements, and defect fixes.

Some customers may prefer a prior instrument software release.  Downgrades can be difficult because, of all the changes and updates in the most current instrument software version. Downgrade are not recommended.

  

發佈日期 版本 版本說明
2019-05-25 K.23.01 Latest release of E7760B instrument software

如何下載

  • Installing instrument software into an E7760B is similar to installing software on a Microsoft Windows based PC.
    • Download the software file onto the instrument (if it is connected to the network)
  • or
    • Download to your PC
    • Transfer the file to the E7760B using a USB storage device
  • For details refer to the E7760B Wideband Transceiver Instrument Software Update Instructions

如何安裝

授權

  • 不需要授權

支援文件

下載

安裝於:

Instrument

作業系統

  • Windows 7

必備檔案

  • 無相關資訊

支援的儀器

  • E7760B SW release K.23.01