您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

RP7950 and RP7960 Series Regenerative Power System Firmware

發佈日期 版本 版本說明
2018-07-03 B.03.01.1191 RP7950 and RP7960 Series Firmware

如何下載

  1. Click the Download button.
  2. Save the file to your computer and note the directory where the file is saved. A firmware update installed over the LAN, GPIB, or USB interface is a file with a .upd extension.
  3. Unzip the file to access the .upd file.

如何安裝

  • From the utility directory or Start menu, start the utility (FWUpdate.exe). The utility will prompt you for the location of the .upd file. Follow the additional prompts to complete the installation. The update may take several seconds to complete and will reboot the instrument. After the update is complete, exit the utility. It is not necessary to re-calibrate the instrument following a firmware-update; however, the instrument may need to be re-secured if it was unsecured to perform the update.

授權

  • 不需要授權

支援文件

外掛軟體/工具程式

下載

安裝於:

Instrument

必備檔案

  • Must have one of the instruments listed

支援的儀器

  • RP7951A, RP7951AT, RP7952A, RP7952AT, RP7953A, RP7961A, RP7962A, RP7963A