Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

M9019A Chassis Firmware

Release Date Version Version Description
2018-06-07 2017 and 2018 See Description.

Description:

The 2017 Firmware version is the first release.

The 2018 Firmware contains enhanced capability for the front panel Trigger Ports such that:

  • When the front panel trigger port is set to Input, the front panel trigger port can connect to any and all PXI_TRIG lines on either of two trigger bus segments 1 or 2 (or both).
  • When the front panel trigger port is set to Output, the front panel trigger port can source the trigger signal from a single PXI_TRIG line on either trigger bus segment 1 or 2.

The only reason to upgrade to the 2018 Firmware version, is if you need the enhanced capability.

Notes:

  • Version 2018 Chassis Firmware only works with PXIe Chassis Family Driver version 1.7.82.1 or above.
  • Version 2017 Chassis Firmware works with any version of the PXIe Chassis Family Driver.
  • To upgrade from version 2017 to version 2018 Chassis Firmware, PXIe Chassis Family Driver version 1.7.82.1 or above must be used to perform the upgrade.
  • To downgrade from version 2018 to version 2017 Chassis Firmware, PXIe Chassis Family Driver version 1.7.82.1 or above must be used to perform the downgrade.

How to Download

  • Click on the download button and save the zip file

How to Install

  • See the PXIe Chassis Family Firmware Guide.

Licensing

  • Does Not Require a License

Supporting Documentation