这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

M9010A Chassis Firmware

发布日期 版本 版本说明
2018-06-07 2017 and 2018 See Description. DO NOT downgrade to these older version if you already have 2019 firmware installed. Chassis with Power Supply hardware version 2 will break if you downgrade it to use with version 2017 or 2018 firmware.

Description:

DO NOT downgrade to these older version if you already have 2019 firmware installed. Chassis with Power Supply hardware version 2 will break if you downgrade it to use with version 2017 or 2018 firmware.

The 2017 Firmware version is the first release.

The 2018 Firmware contains enhanced capability for the front panel Trigger Ports such that:

  • When the front panel trigger port is set to Input, the front panel trigger port can connect to any and all PXI_TRIG lines on either of two trigger bus segments 1 or 2 (or both).
  • When the front panel trigger port is set to Output, the front panel trigger port can source the trigger signal from a single PXI_TRIG line on either trigger bus segment 1 or 2.

The only reason to upgrade to the 2018 Firmware version, is if you need the enhanced capability.

Notes:

  • Version 2018 Chassis Firmware only works with PXIe Chassis Family Driver version 1.7.82.1 or above.
  • Version 2017 Chassis Firmware works with any version of the PXIe Chassis Family Driver.
  • To upgrade from version 2017 to version 2018 Chassis Firmware, PXIe Chassis Family Driver version 1.7.82.1 or above must be used to perform the upgrade.
  • To downgrade from version 2018 to version 2017 Chassis Firmware, PXIe Chassis Family Driver version 1.7.82.1 or above must be used to perform the downgrade.
     

如何下载

  • Click on the download button and save the zip file

如何安装

  • See the PXIe Chassis Family Firmware Guide.

颁发许可证

  • 不要求具有许可证

支持文档