您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

KS8106A REST API Plugin Software

Download and install the latest KS8106A REST API Plugin software.

What's new in version 2.0?

  • We provide supported client libraries for C# and TypeScript.
  • Added support for OpenAPI to allow generating clients for other programming languages.
  • Switch to use the new OpenTAP Annotation system to alleviate differences in property editing between the OpenTAP Editor and the REST-API.
  • Simplification of advanced endpoints.


What changed in version 2.0?

  • Using the REST-API Plugin is now significantly simpler. Previously, lots of boilerplate code was needed to deal with endpoints and parsing JSON responses. In version 2.0, with the help of OpenAPI, that is all abstracted into a user friendly and strongly typed client library. To support this, all endpoints and their JSON content have changed; however, concepts remain the same.
  • "Proxy mode" has been renamed to "SessionManager mode" and the proxy/redirect functionality of Session endpoints through the Proxy/SessionManager has been removed.
發佈日期 版本 版本說明

免費試用版

2020-09-15 2.0.0 Initial 2.x release 2.0.0+fd62a702

如何下載

  1. Click the Continue button
  2. Save or run the Installer

如何安裝

  1. Double-click on the downloaded .tappackage to run the installer

授權

繼續

安裝於:

PC

作業系統

  • Windows 10

必備檔案

  • 無相關資訊

相關連結