这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

EXM Wireless Test Set Software E6640A

Learn more about the measurement applications

This process will update the instrument software and all the measurement applications.  Measurement applications require a license key to enable their functionality. 

Installing the latest instrument software version is encouraged to guarantee your EXM instrument compatibility and performance.

Keysight always recommends using the most current version of the instrument software.  New releases of instrument software keeps your instrument up to date with features, enhancements, and defect fixes.

Some customers may prefer a prior instrument software release.  Downgrades can be difficult because of all the changes and updates in the most current instrument software version.  The document below was written to provide the proper steps should a downgrade be required.

发布日期 版本 版本说明
2018-04-08 E.19.72 Latest release of E6640A instrument Software.

如何下载

  • Installing instrument software into an EXM is similar to installing software on a Microsoft Windows based PC.
    • Download the software file onto the instrument (if it is connected to the network)
  • or
    • Download to your PC
    • Transfer the file to the EXM using a USB storage device
  • For details refer to the EXM Instrument Software Update Instructions

如何安装

颁发许可证

  • 不要求具有许可证

支持文档

下载

安装于:

Instrument

操作系统

  • Windows 7

前提条件

  • 无此信息

支持的仪器

  • E6640A