Here’s the page we think you wanted. See search results instead:

 

Sprechen Sie mit einem Experten

M9537A BIOS Downloads

With upgrading, DO NOT install this version unless you have one previous version installed first. If you skip versions during BIOS upgrade, the M9537A may result in not powering up after the install.


DO NOT downgrade BIOS. Downgrading BIOS will cause unforeseen issue as each version of BIOS is match with specific version of ME firmware and specific windows patches. Please contact Keysight at www.keysight.com/find/contactus if you have the need to downgrade the BIOS.

NOTE: There is not a way to downgrade the M9537A BIOS to older version after you upgraded to SL07.

The M9537A SL07 BIOS has these changes:

  1. Update microcode (from BA to C6) to fix INTEL-SA-00115.
  2. Update ME from 11.8.50.3399 to 11.8.55.3510 to fix INTEL-SA-00125 and INTEL-SA-00141.
  3. Change "Hot Plug Support in DOS" setting (vbios) from Enable to Disable.
  4. Change "Holdoff timer" item range from 0~8 to 0~60 second.
  5. Change "CPU C states" item from Enable to Disable.
Release Date Version Version Description
2020-01-09 SL07 See above. With upgrading, DO NOT install this version unless you have version AG06 installed first. If you skip versions during BIOS upgrade, the M9537A may result in not powering up after the install.

How to Download

  • Click the download button

How to Install

Licensing

  • Does Not Require a License
Download

Installs on:

Instrument

Operating System

  • WES 7 32-bit
  • WES 7 64-bit
  • Win 10 64-bit

Prerequisites

  • Information Not Available

Supported Instruments

  • M9537A