検索された製品ページを表示しています その他の検索結果:

 

お問い合わせ窓口

BT2152A Self-Discharge Analyzer Firmware

リリース バージョン 内容
2017-11-28 A.04.37 Resolves defect causing wiring resistance values to be cleared

ダウンロード方法

  1. Click the Download button.
  2. Save the file to your computer and note the directory where the file is saved. A firmware update installed over the LAN, GPIB, or USB interface is a file with a .upd extension.
  3. Unzip the file to access the .upd file.

インストール方法

  • From the utility directory or Start menu, start the utility FWUpdate.exe (a link to this utility can be found directly below). The utility will prompt you for the location of the .upd file. Follow the additional prompts to complete the installation. The update may take several seconds to complete and will reboot the instrument. After the update is complete, exit the utility. It is not necessary to re-calibrate the instrument following a firmware-update; however, the instrument may need to be re-secured if it was unsecured to perform the update.

ライセンス

  • ライセンス不要

説明資料

アドオン・ソフトウェア/ユーティリティ

ダウンロード

インストール:

Instrument

OS

  • Windows 7
  • Windows XP
  • Windows 10

前提条件

  • ドキュメントはありません

対象測定器

  • BT2152A