Here’s the page we think you wanted. See search results instead:

 

Discutez avec un expert

BT2152A/B Self-Discharge Analyzer Firmware

BT2152A/B Self-Discharge Analyzer Firmware

BT2152A/B Self-Discharge Analyzer Firmware

Release Date Version Version Description
2019-06-19 A.04.76 Adds support for BT2152B, in situ resistance calibration, median-based analysis, and other enhancements and fixes

How to Download

  1. Click the Download button.
  2. Save the file to your computer and note the directory where the file is saved. A firmware update installed over the LAN, GPIB, or USB interface is a file with a .upd extension.
  3. Unzip the file to access the .upd file.

How to Install

  • From the utility directory or Start menu, start the utility FWUpdate.exe (a link to this utility can be found directly below). The utility will prompt you for the location of the .upd file. Follow the additional prompts to complete the installation. The update may take several seconds to complete and will reboot the instrument. After the update is complete, exit the utility. It is not necessary to re-calibrate the instrument following a firmware-update; however, the instrument may need to be re-secured if it was unsecured to perform the update.

Licensing

  • Does Not Require a License

Supporting Documentation

Add-On Software / Utilities

Download

Installs on:

Instrument

Operating System

  • Windows 7
  • Windows XP
  • Windows 10

Prerequisites

  • Information Not Available

Supported Instruments

  • BT2152A, BT2152B