Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discuter avec un expert

BT2152A/B Self-Discharge Analyzer Firmware

BT2152A/B Self-Discharge Analyzer Firmware

BT2152A/B Self-Discharge Analyzer Firmware

Date de mise en circulation Version Description de la version
2019-06-19 A.04.76 Adds support for BT2152B, in situ resistance calibration, median-based analysis, and other enhancements and fixes

Comment télécharger

  1. Click the Download button.
  2. Save the file to your computer and note the directory where the file is saved. A firmware update installed over the LAN, GPIB, or USB interface is a file with a .upd extension.
  3. Unzip the file to access the .upd file.

Comment installer

  • From the utility directory or Start menu, start the utility FWUpdate.exe (a link to this utility can be found directly below). The utility will prompt you for the location of the .upd file. Follow the additional prompts to complete the installation. The update may take several seconds to complete and will reboot the instrument. After the update is complete, exit the utility. It is not necessary to re-calibrate the instrument following a firmware-update; however, the instrument may need to be re-secured if it was unsecured to perform the update.

Autorisation d'exploitation

  • Ne requiert aucune licence

Document d'appui

Logiciels additionels/utilités

Téléchargez

S'installe sur:

Instrument

Système d'exploitation

  • Windows 7
  • Windows XP
  • Windows 10

Préalables

  • Information non-disponible

Instruments appuyés

  • BT2152A, BT2152B