这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

BT2152A/B Self-Discharge Analyzer Firmware

BT2152A/B Self-Discharge Analyzer Firmware

BT2152A/B Self-Discharge Analyzer Firmware

发布日期 版本 版本说明
2019-06-19 A.04.76 Adds support for BT2152B, in situ resistance calibration, median-based analysis, and other enhancements and fixes

如何下载

  1. Click the Download button.
  2. Save the file to your computer and note the directory where the file is saved. A firmware update installed over the LAN, GPIB, or USB interface is a file with a .upd extension.
  3. Unzip the file to access the .upd file.

如何安装

  • From the utility directory or Start menu, start the utility FWUpdate.exe (a link to this utility can be found directly below). The utility will prompt you for the location of the .upd file. Follow the additional prompts to complete the installation. The update may take several seconds to complete and will reboot the instrument. After the update is complete, exit the utility. It is not necessary to re-calibrate the instrument following a firmware-update; however, the instrument may need to be re-secured if it was unsecured to perform the update.

颁发许可证

  • 不要求具有许可证

支持文档

附加的软件/实用程序

下载

安装于:

Instrument

操作系统

  • Windows 7
  • Windows XP
  • Windows 10

前提条件

  • 无此信息

支持的仪器

  • BT2152A, BT2152B