Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discuter avec un expert

Keysight i3070 09.01pa Software Patchs

This software patch should only be installed on Microsoft Windows systems with i3070 09.01p software release. Please refer to Release Notes for details.
 

Date de mise en circulation Version Description de la version
2017-07-24 09.01pa Contains various enhancements and support for RoHS implementation. Refer to release notes for more information.

Comment télécharger

  • Click the "Download" button and save file to local hard drive.

Comment installer

  • Follow these steps to install the 09.01pa software patch:
    1. Save the Keysight_i3070_0901pa.exe file to your hard disk.
    2. Close all open programs.
    3. Double-click Keysight_i3070_0901pa.exe
    4. Follow the on-screen instructions for installation.
    5. To validate that the software was installed correctly:
  • a) On the Start menu, select Programs > Agilent ICT > Korn Shell

    b) In the Korn Shell window, type version and press Enter. The display should show Keysight i3070 09.01pa 1116 WN
     

Autorisation d'exploitation

  • Requiert une licence
Téléchargez

S'installe sur:

PC

Système d'exploitation

  • Windows 7

Préalables

  • Information non-disponible