这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

Keysight i3070 09.01pa Software Patchs

This software patch should only be installed on Microsoft Windows systems with i3070 09.01p software release. Please refer to Release Notes for details.
 

发布日期 版本 版本说明
2017-07-24 09.01pa Contains various enhancements and support for RoHS implementation. Refer to release notes for more information.

如何下载

  • Click the "Download" button and save file to local hard drive.

如何安装

  • Follow these steps to install the 09.01pa software patch:
    1. Save the Keysight_i3070_0901pa.exe file to your hard disk.
    2. Close all open programs.
    3. Double-click Keysight_i3070_0901pa.exe
    4. Follow the on-screen instructions for installation.
    5. To validate that the software was installed correctly:
  • a) On the Start menu, select Programs > Agilent ICT > Korn Shell

    b) In the Korn Shell window, type version and press Enter. The display should show Keysight i3070 09.01pa 1116 WN
     

颁发许可证

  • 要求具有许可证
下载

安装于:

PC

操作系统

  • Windows 7

前提条件

  • 无此信息