这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

自动化测试平台开发人员系统 2017

Keysight KS8400A 自动化测试平台(TAP)开发人员系统 2017 版本提供了功能强大、灵活并可扩展的测试序列和测试计划生成等功能,可以优化您的测试软件开发和总体性能。Keysight TAP 是基于 Microsoft .NET 的现代化应用软件,能够独立使用,也能够与更高级的测试可执行软件环境配合运行。TAP 不只是另一种编程语言,它还能充分发挥 C# 和强大的 Microsoft Visual Studio 的优势。在 TAP 平台上,您可以构建自己的测试解决方案,并且通过利用现有的软件开发工具和基础设施最大限度提高自身团队的工作效率。

发布日期 版本 版本说明
2019-05-28 9.1.3 Now built using OpenTAP engine
  • Now built on OpenTAP  open-source test sequencer
  • Two Versions Available: Enterprise Product and now Community Edition for non-commercial users
  • See Release Notes for other features, improvements, and bug fixes

如何下载

  1. Click the Download button.
  2. Save or Run the installer.

如何安装

  1. Double-Click the .exe file

颁发许可证

  • 要求具有许可证

支持文档

下载

安装于:

PC

操作系统

  • Windows 8
  • Windows 7
  • Windows 10

前提条件

  • 无此信息

相关链接

2018-12-20 8.8.78 TAP 2018 Update 7 Developer System
  • Improved filtering and bulk updates of Test Plans
  • Added Select All options for Sweep Loop Parameter Settings
  • "Dot" display is replaced with Dropdown for Resource Settings
  • Performance improvements for SQLite database
  • Performance improvements for Parallel Step
  • See Release Notes for other features, improvements, and bug fixes

如何下载

  • 1. Click the Download button.
  • 2. Save or Run the installer.

如何安装

  • Double-click on the downloaded software file to run the installer
     

颁发许可证

  • 要求具有许可证

支持文档

下载

安装于:

PC

操作系统

  • Windows 8
  • Windows 7
  • Windows 10

前提条件

相关链接

2018-11-29 8.7.284 TAP 2018 Update 6 Developer System
  • Right-click menu allows for Enable/Disable of all Test Steps in Tes Plan Panel
  • Added Package Cache for install performance improvements
  • TestPlan doesn’t load anymore if required packages are missing to prevent accidental changes
  • TAP GUI performance improvments for large Test Plans
  • Perfomance improvements for license validation
  • Various other bug and performance fixes. See Release Notes for more deteails.

如何下载

  • 1. Click the Download button.
  • 2. Save or Run the installer.

如何安装

  • Double-click on the downloaded software file to run the installer

颁发许可证

  • 要求具有许可证

支持文档

下载

安装于:

PC

操作系统

  • Windows 8
  • Windows 7
  • Windows 10

前提条件

相关链接

2018-11-08 8.6.440 TAP 2018 Update 5 Developer System

This release includes bugfixes and infrastructural improvements as well as a few GUI enhancements. See the Release Notes for full details.

如何下载

  • 1. Click the Download button.
  • 2. Save or Run the installer.

如何安装

  • Double-click on the downloaded software file to run the installer
     

颁发许可证

  • 要求具有许可证

支持文档

下载

安装于:

PC

操作系统

  • Windows 8
  • Windows 7
  • Windows 10

前提条件

相关链接

2018-08-16 8.5.456 TAP 2018 Update 4 Developer System

Highlights:

  • Resources can be opened when a given test step needs them, not when a test plan starts
  • PackageDependency versions now update when creating a package
  • Enable/Disable of SCPI logging
  • Resource properties can have placeholder arguments, so they can map to any compatible resource at execution time
  • Using Shift to select multiple test steps no longer expands test steps that are collapsed
  • The behavior of the Repeat button simplified
  • Scrollbar now follows selected step when scrolling up with arrow keys
  • Fixed incompatibility issue with Dependency Resolution with .NET 4.7.1 installed
  • Fixed issue with installing packages from network drive
  • Numberous other features, improvements, and bug fixes (see Release Notes)

如何下载

  • 1. Click the Download button.
  • 2. Save or Run the installer.

如何安装

  • Double-click on the downloaded software file to run the installer

颁发许可证

  • 要求具有许可证

支持文档

下载

安装于:

PC

操作系统

  • Windows 8
  • Windows 7
  • Windows 10

前提条件

相关链接

2018-07-04 8.4.566 TAP 2018 Update 3 Developer System

Includes numerous performance improvements and bug fixes

如何下载

  • 1. Click the Download button.
  • 2. Save or Run the installer.

如何安装

  • Double-click on the downloaded software file to run the installer

颁发许可证

  • 要求具有许可证

支持文档

2018-04-14 8.3.522 TAP 2018 Update 2 Developer System

TAP 2018 Update 2 Developer System Includes:

  • Support that Test Steps can run actions after Test Step Run() completes.
  • Possibility to jump to any Test Step at the current hierarchy level when you hit a break point
  • Bundles view in Package Manager GUI
  • Allow exporting to databases in Run Explorer
  • Many other improvements and bug fixes

如何下载

  • 1. Click the Download button.
  • 2. Save or Run the installer.

如何安装

  • Double-click on the downloaded software file to run the installer
     

颁发许可证

  • 要求具有许可证

支持文档

2018-02-13 8.2.510 TAP 2018 Update 1 Developer System

TAP 2018 Update 1 Developer System Includes:

  • Support for multiple group levels in Step Settings
  • Support for switch matrix rows and columns in the Connection Settings
  • Significant performance improvements in the Log Panel
  • Search highlighting in the Log Panel
  • More than 80 other improvements and bug fixes

如何下载

  • 1. Click the Download buttonn.
  • 2. Save or Run the installer.

如何安装

  • Double-click on the downloaded software file to run the installer

颁发许可证

  • 要求具有许可证

支持文档

2017-11-27 8.1.318 TAP 2018 Developer System

TAP 2018 Developer System Includes:

  • Support for docking and undocking of windows/panels in the TAP GUI
  • Support for custom GUI panels as plugins, e.g. make your own manufacturing UI or live data views.
  • Support for plugins stored in custom folders.
  • TAP Engine, CLI and Package Manager CLI, now .NET Standard 2.0 compliant.
  • TAP 2018 can be installed side by side with your existing TAP 2017 version.
  • Numerous other bug fixes and performance improvements.

如何下载

  1. Click the Download button
  2. Save or run the installer.

如何安装

  • Double-click on downloaded software file to run the installer.

颁发许可证

  • 要求具有许可证

支持文档

2017-06-29 7.4.79.0 TAP 2017 Update 2

TAP 2017 Update 2 includes:

  • Allow instruments to use other instruments as resources.
  • Support for signing assemblies when they are packaged.
  • Package Manager GUI now supports searching across plugin packages.
  • Package Manager can now source packages from multiple repositories.
  • Check for dependencies between plugin packages during uninstall.
  • Test Steps can now implement IResource (useful when used with Keysight Measurement Framework, KMF).
     

如何下载

  1. Click the Download button
  2. Save or run the installer.

如何安装

  • Double-click on downloaded software file to run the installer.
     

颁发许可证

  • 要求具有许可证
2017-05-10 7.3.165.0 See description above.

TAP 2017 Update 1 includes:

  • PostgreSQL databases now supported for Result Listeners.
  • External parameters can now be imported/exported to a file, also via CLI.
  • Result Viewer can now import data directly from csv files.
  • Search field in Run Explorer now supports auto completion.
  • Performance improvements in Engine and GUI.
  • Package Manager shows information about license requirements, provides simplified plugin installation process
  • Compare Test Plans feature now make use of external compare tool.
  • Combined installer for both 32-bit and 64-bit.
  • Improved help content
  • Resolved license issues
  • … and more than 200 other improvements and fixes.
     

如何下载

  1. Click the Download button
  2. Save or run the installer.

如何安装

  • Double-click on downloaded software file to run the installer

颁发许可证

  • 要求具有许可证
2017-02-22 7.0.1098.0 Updates to support plugin licensing.

Test sequencer software with timing analyzer, result viewer, and other useful tools for test automation development.

如何下载

  1. Click the Download button
  2. Save or run the installer.

如何安装

  • Double-click on downloaded software file to run the installer

颁发许可证

  • 要求具有许可证
2016-12-22 7.0.1089.0 Bug fixes.

Test sequencer software with timing analyzer, result viewer, and other useful tools for test automation development.

如何下载

  1. Click the Download button
  2. Save or run the installer.

如何安装

  • Double-click on downloaded software file to run the installer

颁发许可证

  • 要求具有许可证
2016-10-24 7.0.1025.0 最初版本

测试序列发生器软件配有计时分析软件、结果查看器和其他实用工具,适用于自动化测试开发。

如何下载

  1. 点击下载按钮
  2. 保存或运行安装程序

如何安装

  • 双击下载的软件文件,运行安装程序

颁发许可证

  • 要求具有许可证
下载

安装于:

PC

操作系统

  • Windows 8
  • Windows 7
  • Windows 10

前提条件

相关链接