This page contains an .iso file, which can be used to burn a DVD. 
For the normal download file (.exe), navigate to the Keysight Instrument Control Bundle Download page.
 

 

This no cost download includes all three Keysight instrument control software packages. Download this bundle for simple installation and flexible instrument connectivity.

The download bundle includes:

  • IO Libraries Suite: for discovering and connecting instruments.
  • Command Expert: for building instrument control applications.
  • BenchVue Platform: for viewing and capturing instrument data with no programming.
Keysight recommends using the most current version, which includes the most up-to-date bug fixes and security patches available.
Release Date Version Version Description
2024-01-16 1.2024 This .iso file can be burned onto a DVD for installation in secure labs or labs without internet connectivity. Includes IOLS 2023 Update 1, BenchVue Complete Control Collection (CCC) 2023.2 Command Expert 2023 and offline command sets from November 2023.
Release Date Version
2024-01-16 1.2024
Version Description
This .iso file can be burned onto a DVD for installation in secure labs or labs without internet connectivity. Includes IOLS 2023 Update 1, BenchVue Complete Control Collection (CCC) 2023.2 Command Expert 2023 and offline command sets from November 2023.

Support for Windows 11 added for IO Libraries Suite, Command Expert and BenchVue classic and PathWave BenchVue applications.

Updated .NET Framework requirement in Command Expert 2023 from version 3.5 to version 4.5.2

BenchVue Completely Control Collection (CCC) installer includes its prerequisites, platform and various BenchVue classic and PathWave BenchVue standalone applications.

Visit the BenchVue Complete Control Collection (CCC) download page to obtain only the BenchVue CCC offline installer that has the size of 4.8 GB.

 

 

How to Download

  1. Click the download button
  2. Select the .iso file
  3. Save to your online computer
  4. Use a DVD burner or other tools to write the .iso file on your online computer into a double-sided DVD, secure harddrive or read-only drive. 
  5. Use the double-sided DVD, secure harddrive or read-only drive to install these three software in the offline computer(s) or secure lab environment.

How to Install

  • Use a tool to burn the .iso file to a blank double-sided DVD. As these tools mentioned in Step 4 above are third-party tools, support will not be provided by Keysight Technologies, Inc.

  • Or you can also choose to right-click on the .iso file and Mount the .iso image virtually in Windows that that have that feature enabled to access the installers without burning it onto a DVD. Please look online on how to do this.

  • Double-sided DVD may be required as this ISO file size is close to 8 GB and most single-sided DVDs only hold about 4 GB.

Licensing

  • In general: No cost, Perpetual, Floating (unlimited copies) license (no activation required)
  • Advanced features in BenchVue Classic applications and PathWave BenchVue applications have additional licensing requirements. Refer to each application's documentation and download page.

Installs on: PC

Operating System

  • Windows 11
  • Windows 10

Prerequisites

  • Not aware of any prerequisites

Latest BenchVue platform versions are supported only on Windows 10 and thus the supported OS's are listed to be only Windows 10 eventhough IO Libraries Suite 2022 U2 and Command Expert 2022 are supported on Windows 8 and Windows 7.

.NET 3.5 Framework is no longer required for IO Libraries Suite 2022 U2 but it is still required for Command Expert 2022. It is best to install it on Windows 10 images that have this feature pre-installed by your IT department, especially in secure environments without internet connection.

BenchVue Completely Control Collection (CCC) installer includes its prerequisites, platform and various BenchVue classic and PathWave BenchVue standalone applications.

 

How to Download

  1. Click the download button
  2. Select the .iso file
  3. Save to your computer

How to Install

  • Use a tool to burn the .iso file to a blank DVD.

  • Or you can also choose to right-click on the .iso file and Mount the .iso image virtually in Windows that that have that feature enabled to access the installers without burning it onto a DVD. Please look online on how to do this.

  • Double-sided DVD may be required as this ISO file size is close to 6 GB and most single-sided DVDs only hold about 4 GB.

Licensing

  • IO Libraries Suite and Command Expert do not require a license
  • BenchVue applications do require licenses

Installs on: PC

Operating System

  • Windows 10

Prerequisites

  • Windows 10 OS image with .NET Framework 3.5 preinstalled.

BenchVue 2020 Platform is supported only on Windows 10 and thus the supported OS's are listed to be only Windows 10 eventhough IO Libraries Suite 2020 and Command Expert 2019 are supported on Windows 8 and Windows 7.

.NET 3.5 Framework is required for IO Libraries Suite 2020 so it is best to install it on Windows 10 images that have this feature pre-installed by your IT department, especially in secure environments without internet connection.

BenchVue application installer .exe's are included in a separate folder within the .iso image. These application installers were the latest versions available in May 2020.

How to Download

  1. Click the download button
  2. Select the .iso file
  3. Save to your computer

How to Install

  • Use a tool to burn the .iso file to a blank DVD.

  • Or you can also choose to right-click on the .iso file and Mount the .iso image virtually in Windows that that have that feature enabled to access the installers without burning it onto a DVD. Please look online on how to do this.

  • Double-sided DVD may be required as this ISO file size is close to 5 GB and most single-sided DVDs only hold about 4 GB.

Licensing

  • Does Not Require a License

Installs on: PC

Operating System

  • Windows 10

Prerequisites

  • Windows 10 OS image with .NET Framework 3.5 preinstalled.

Supported Instruments

  • See list for BenchVue 2020 apps and Command Expert 2019.

How to Download

  1. Click the download button
  2. Select the .iso file
  3. Save to your computer

How to Install

  • Use a tool to burn the .iso file to a blank DVD.

Licensing

  • Does Not Require a License

Installs on: PC

Operating System

  • Windows 8
  • Windows 7
  • Windows 10

Prerequisites

  • None required.

Supported Instruments

  • See list for BenchVue 2019 apps and Command Expert 2019/2018.

How to Download

  1. Click the download button
  2. Select the .iso file
  3. Save to your computer

How to Install

  • Use a tool to burn the .iso file to a blank DVD.

Licensing

  • Does Not Require a License

Installs on: PC

Operating System

  • Windows 8
  • Windows 7
  • Windows 10

Prerequisites

  • Information Not Available

How to Download

  1. Click the download button
  2. Select the .iso file
  3. Save to your computer

How to Install

  • Use a tool to burn the .iso file to a blank DVD.

Licensing

  • Does Not Require a License

Installs on: PC

Operating System

  • Windows 8
  • Windows 7
  • Windows 10

Prerequisites

  • No specific prerequisites

How to Download

  1. Click the download button
  2. Select the .iso file
  3. Save to your computer

How to Install

  • Use a tool to burn the .iso file to a blank DVD.

Licensing

  • Does Not Require a License

Installs on: PC

Operating System

  • Windows 8
  • Windows 7
  • Windows 10

Prerequisites

  • No specific prerequisites

How to Download

  1. Click the download button
  2. Select the .iso file
  3. Save to your computer

How to Install

  • Use a tool to burn the .iso file to a blank DVD.

Licensing

  • Does Not Require a License

Installs on: PC

Operating System

  • Windows 8
  • Windows 7
  • Windows 10

Prerequisites

  • No specific prerequisites

How to Download

  1. Click the download button
  2. Select the .iso file
  3. Save to your computer

How to Install

  • Use a tool to burn the .iso file to a blank DVD.

Licensing

  • Does Not Require a License

Installs on: PC

Operating System

  • Windows 8
  • Windows 7
  • Windows 10

Prerequisites

  • No specific prerequisites

How to Download

  1. Click the download button
  2. Select the .iso file
  3. Save to your computer

How to Install

  • Use a tool to burn the .iso file to a blank DVD.

Licensing

  • Does Not Require a License

Installs on: PC

Operating System

  • Windows 8
  • Windows 7
  • Windows 10

Prerequisites

  • No specific prerequisites

How to Download

  1. Click the download button
  2. Select the .iso file
  3. Save to your computer

How to Install

  • Use a tool, such as www.imgburn.com, to burn the .iso file to a blank DVD.

Licensing

  • Does Not Require a License

Installs on: PC

Operating System

  • Windows 8
  • Windows 7
  • Windows 10

Prerequisites

  • No specific prerequisites

Supported Instruments

  • All instruments

How to Download

  1. Click the download button
  2. Select the .iso file
  3. Save to your computer

How to Install

  • Use a tool, such as www.imgburn.com, to burn the .iso file to a blank DVD.

Licensing

  • Does Not Require a License

Installs on: PC

Operating System

  • Windows 8
  • Windows 7
  • Windows 10

Prerequisites

  • No specific prerequisites.

Supported Instruments

  • All instruments

How to Download

  1. Click the download button
  2. Select the .iso file
  3. Save to your computer

How to Install

  • Use a tool, such as www.imgburn.com, to burn the .iso file to a blank DVD.

Licensing

  • Does Not Require a License

Installs on: PC

Operating System

  • Windows 8
  • Windows 7
  • Windows 10

Prerequisites

  • No specific prerequisites.

Supported Instruments

  • All instruments

How to Download

  1. Click the download button
  2. Select the .iso file
  3. Save to your computer

How to Install

  • Use a tool, such as www.imgburn.com, to burn the .iso file to a blank DVD.

Licensing

  • Does Not Require a License

Installs on: PC

Operating System

  • Windows 8
  • Windows 7
  • Windows 10

Prerequisites

  • No specific prerequisites

Supported Instruments

  • All instruments

How to Download

  1. Click the download button
  2. Select the .iso file
  3. Save to your computer

How to Install

  • Use a tool, such as www.imgburn.com, to burn the .iso file to a blank DVD.

Licensing

  • Does Not Require a License

Installs on: PC

Operating System

  • Windows 8
  • Windows 7
  • Windows 10

Prerequisites

  • No specific prerequisites

Supported Instruments

  • All instruments

How to Download

  1. Click the download button
  2. Select the .iso file
  3. Save to your computer

How to Install

  • Use a tool, such as www.imgburn.com, to burn the .iso file to a blank DVD.

Licensing

  • Does Not Require a License

Installs on: PC

Operating System

  • Windows 8
  • Windows 7
  • Windows 10

Prerequisites

  • No specific prerequisites

Supported Instruments

  • All instruments
SHOW MORE