Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

M9169E PXI Programmable Step Attenuator Module Firmware

1. Open command prompt.

2. Point to the directory of the firmware files (.exe) where it located. The firmware files name format is “M9169E_A_00_01.exe”.

3.Then type in the command, example: M9169E_A_00_01 PXI23::12::0::INSTR. The module’s VISA address can be obtained from Keysight Connection Expert or Soft Front Panel.

4. Restart the instrument after the firmware upgrade is completed.

No previous versions available.