検索された製品ページを表示しています その他の検索結果:

 

お問い合わせ窓口

FieldFox Handheld Microwave Analyzer Firmware Release Notes (N991xA, N992xA, N993xA, N995xA, N996xA)


FieldFox firmware revisions are listed below. 

 

Version Release Date Notes
A.11.52 Jan 6, 2020
  • 5GNR Support Added to FieldFox
A.11.31 Nov. 12, 2019
  • B models won't connect to VSA without B04 or B10 license
A.11.27 Sep. 17, 2019
  • Addition of the FieldFox Self-Test program
A.11.26 Jul 11, 2019
  • Support for B Model Products
A.11.03 May 6, 2019
  • MMEM:STOR:SNP missing from Wilson
  • N9912A: SA mode TG not property initialized for power
  • FOPS: 1st point of trace can be incorrect
A.11.02 Mar 1, 2019
  •  NF: Enhancement request - frequency annotation
  •  Center Frequency Not Properly Coupled to Start-Stop Frequencies For Converter DUT Types
  •  LO Frequency Not Properly Coupled Start-Stop Frequencies for Upconverter DUT Type
  •  Standby operation fails (NullReferenceException reported to the screen) if no VVS license installed on Carson and later models.

 

A.10.34 Dec 18, 2018
  • Installer does not handle install package files that have the read-only bit set.
  • NA mode: Marker table readout not legible in 2 trace overlay mode when one trace has marker bandwidth search turned on
  • TSS: recalling a saved pulse definition .xml file results in a NullReferenceException 
A.10.33 Sep 28, 2018
  • File Management -- choosing "Select Files" on an empty file list crashes unit
A.10.31 Aug 09, 2018
  • Crash when setting NA trace through Settings page
A.10.30 June 26, 2018
  • Option 356 Noise Figure
A.10.20 May 9, 2018
  • Various Bug fixes
A.10.18 Mar 05, 2018
  • channel scanner "pause" fix
A.10.17 Feb 13, 2018
  • Forward Response and Reverse Response cals broken in IQA release
  • Power Sensors: newest power sensor firmware incompatible with FieldFox firmware A.10.0x and A.10.1x

Fixed with A.10.16:

  • Customer reports disconnect-reconnect failure on thermocouple power sensors
  • ERTA: Input (SrcSide) cable corr is applied to B; should be applied to R
  • DTF -- recalling .csv file that has units set to "feet" causes incorrect x axis values both on the unit and via Datalink
  • Japanese, Chinese, and Korean fonts are missing
  • System, System Configuration, Options, Show Options -- displayed options columns are mis-sorted
A.10.15 Jan 29, 2018
  • Frequency domain and time domain measurements up to 10 MHz of analysis bandwidth
  • Customize display with up to 4 simultaneous and multi-domain measurement views
  • Requires spectrum analyzer mode (not supported on model N9912A)
A.10.01 Sep 12, 2017
  • VSA Support
  • No Support for DataLink at this time. Use the A.09.64 version for DataLink Support.
A.09.64 Aug 3, 2017 Print, Select Files for Printing, can't edit the row and column fields
A.09.62 Jun 5, 2017
  • Power meter mode with peak sensor
  • Print doesn't work with CPU2 units
  • GPS C/No Averaging Feature
  • GPS 1/sec update rate
  • Add cable FSJ4-50B
  • Power Sensor U2022XA H50 and U8489A support
  • Additional calkits
  • Various Power Meter fixes, including "device clear"
A.09.60 Mar. 20, 2017 No info at this time.
A.09.57 January 27, 2017

Installer on OF SD card does not run after programing QSPI with model/serial clear

Enhanced Response calibration not working with ECal unit

FieldFox with CPU2 self-assigns IP address (169.x.x.x) when connected to network with DHCP server

Wrong data in cable file DTF cable

     

 

リリース バージョン 内容
2019-11-12 A.11.31 Latest Software version for FieldFox products

ダウンロード方法

  • Click the download button, select file and save.

インストール方法

  • NOTE! Please backup all user state files to computer or USB flash drive before updating to latest firmware revision.
  • See firmware update supporting documentation for installation process.

ライセンス

  • ライセンス不要

説明資料

ダウンロード

インストール:

Instrument

前提条件

  • ドキュメントはありません

対象測定器

  • N991xA, N992xA, N993xA, B Models N995xA, N996xA analyzers with CPU2
2019-07-11 A.11.26 Latest Software version for all FieldFox products

ダウンロード方法

  • Click the download button, select file and save.

インストール方法

  • NOTE! Please backup all user state files to computer or USB flash drive before updating to latest firmware revision.
  • See firmware update supporting documentation for installation process.

ライセンス

  • ライセンス不要

説明資料

ダウンロード

インストール:

Instrument

前提条件

  • ドキュメントはありません

対象測定器

  • N991xA, N992xA, N993xA, B Models N995xA, N996xA analyzers with CPU2
2019-05-06 A.11.03 Latest software version for all FieldFox models

ダウンロード方法

  • Click the download button, select file and save.

インストール方法

  • NOTE! Please backup all user state files to computer or USB flash drive before updating to latest firmware revision.
  • See firmware update supporting documentation for installation process.

ライセンス

  • ライセンス不要

説明資料

ダウンロード

インストール:

Instrument

前提条件

  • ドキュメントはありません

対象測定器

  • N991xA, N992xA, N993xA, N995xA, N996xA analyzers with CPU2