Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

M9037A BIOS Downloads

Release Date Version Version Description
2015-11-05 AG09 See description above.

The AG09 BIOS corrects or improves the following problems found with the previous version:

  • Allow PCIe devices to have a larger memory footprint.
  • Support 16 GB device BAR and increase system memory to 512 GB.
  • Allow operation with a wider range of USB devices.
  • Resolve issue with pressing ESC in the BIOS boot menu.
  • Resolved USB connection issue with Keysight N6700B.
  • Special case addition to the white list (Ven=0E80, Dev=190C).
     

How to Download

  • Click on the download button

How to Install

Licensing

  • Does Not Require a License
Download

Installs on:

Instrument

Operating System

  • WES 7 32-bit
  • WES 7 64-bit

Prerequisites

  • No specific prerequisites

Supported Instruments

  • M9037A
2015-01-21 AG08 See description below.

The AG08 BIOS corrects or improves the following problems found with the previous version:

  • The BIOS screen now displays Keysight instead of Agilent.
  • In the "Setup Utility" in the "Main Tab" the field "Boot Source" is added. The legal values for this field are 0x0 = Primary BIOS, 0x1 = Backup BIOS, or External BIOS.
  • In the "Setup Utility" in the "Main Tab" the field "BIOS Version" will now display the version of the "Boot Source".
  • If the "Quiet Boot" field is disabled then the POST (Power On Self-Test) results will now be displayed at Restart.
  • When the hold off timer is enabled the sequence is now PERST# => Hot Reset => Delay => Enumerate. The old sequence was PERST# => Delay => Hot Reset => Enumerate.
  • Both the HDD-Master password and the HDD-User password are removed from the Setup Utility Security tab.
  • Changed the SATA port 0 Gen3 receiver DTLE value from 0x2 to 0x6 to fix Intel SSC drop issue.

How to Download

  • Click on the download button

How to Install

Licensing

  • Does Not Require a License
Download

Installs on:

Instrument

Operating System

  • WES 7 32-bit
  • WES 7 64-bit

Prerequisites

  • Information Not Available

Supported Instruments

  • M9037A
2014-03-26 AG07 Original shipping version.

How to Download

  • Click on the download button

How to Install

Licensing

  • Does Not Require a License
Download

Installs on:

Instrument

Operating System

  • WES 7 32-bit
  • WES 7 64-bit

Prerequisites

  • Information Not Available

Supported Instruments

  • M9037A