您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

L4411A DMM Firmware

發佈日期 版本 版本說明
2015-06-08 2.41 L4411A Firmware Update Revision 2.41.

如何下載

  1. Download and install the L4411A Firmware Update Utility located in the "Add-On Software/Utilities" section at the bottom of this page. If you already have the Firmware Update Utility installed on your computer, skip this step.
  2. Use the Download button to download the Keysight L4411A Firmware.
  3. Unzip the Keysight L4411A Firmware file, making note of where you store the unzipped file.
  4. Open the Firmware Update Utility (Start -> Programs -> Keysight -> Firmware Update Utility).
  5. Click Next.

如何安裝

  1. Click Browse and locate the firmware update file that you unzipped. Highlight the file and select Open.
  2. Click Next.
  3. Select the I/O interface (GPIB, LAN, or USB) that connects your DMM to your PC.
  4. Choose the settings necessary for communication (GPIB address, IP address, USB ID).
  5. Click Update. NOTE: This update will take several minutes and the DMM will display status messages and automatically reboot when completed. DO NOT cycle or interrupt power to the DMM during the update process.
  6. After this is completed, exit the update utility.
  7. Refer to the DMM front panel and note if there are any errors (the ERROR light will be on in the display).
  8. The update process is now complete.

授權

  • 不需要授權

支援文件

外掛軟體/工具程式

下載

安裝於:

Instrument

必備檔案

  • No specific prerequisites.

支援的儀器

  • L4411A