Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discuter avec un expert

PA2200 Series Firmware

Before updating instrument firmware, remove power from the power channel inputs. You may leave the connectors in place, but there should be no current or voltage signals going into the power analyzer.

Date de mise en circulation Version Description de la version
2016-12-23 2.34 Adds enhanced harmonic analysis capabilities and resolves minor defects.

Comment télécharger

  • Click the download button and either save the file to a USB flash drive or save the file to your computer and then copy it to a USB flash drive.

Comment installer

  • To perform the firmware update:
    1. Put the USB flash drive with the *.KUP file into one of the front-panel USB ports.
    2. Press [Utility] > File Explorer.
    3. Use the first softkey and the Entry knob to browse to the *.KUP file on the USB drive.
    4. Press the Load File softkey.
      ­
  • The firmware update utility will run, and the instrument will cycle power to start running the new firmware.

Autorisation d'exploitation

  • Ne requiert aucune licence

Document d'appui

Téléchargez

S'installe sur:

Instrument

Préalables

  • None

Instruments appuyés

  • PA2201A, PA2203A