이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

PA2200 Series Firmware

Before updating instrument firmware, remove power from the power channel inputs. You may leave the connectors in place, but there should be no current or voltage signals going into the power analyzer.

릴리스 날짜 버젼 버전 설명
2017-03-15 2.37 Changes the remote response to the Continuous Whole-Cycle Analysis (CWA) query if the measurement has not been initiated or was unable to complete, and resolves minor defects.

다운로드 방법

  • Click the download button and either save the file to a USB flash drive or save the file to your computer and then copy it to a USB flash drive.

설치 방법

  • To perform the firmware update:
    1. Put the USB flash drive with the *.KUP file into one of the front-panel USB ports.
    2. Press [Utility] > File Explorer.
    3. Use the first softkey and the Entry knob to browse to the *.KUP file on the USB drive.
    4. Press the Load File softkey.
      ­
  • The firmware update utility will run, and the instrument will cycle power to start running the new firmware.

라이센스

  • 라이센스 필요 없음

지원 문서

다운로드

설치 위치:

Instrument

사전 조건

  • 사용 가능한 정보 없음

지원되는 계측기

  • PA2201A, PA2203A