您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

PA2200 系列韌體

更新儀器韌體前,請先將電源通道輸入的電源移除。連接器可以繼續插著,但電源分析儀不可以有電流或電壓信號流入。

發佈日期 版本 版本說明
2017-03-15 2.37 Changes the remote response to the Continuous Whole-Cycle Analysis (CWA) query if the measurement has not been initiated or was unable to complete, and resolves minor defects.

如何下載

  • Click the download button and either save the file to a USB flash drive or save the file to your computer and then copy it to a USB flash drive.

如何安裝

  • To perform the firmware update:
    1. Put the USB flash drive with the *.KUP file into one of the front-panel USB ports.
    2. Press [Utility] > File Explorer.
    3. Use the first softkey and the Entry knob to browse to the *.KUP file on the USB drive.
    4. Press the Load File softkey.
      ­
  • The firmware update utility will run, and the instrument will cycle power to start running the new firmware.

授權

  • 不需要授權

支援文件

下載

安裝於:

Instrument

必備檔案

  • 無相關資訊

支援的儀器

  • PA2201A, PA2203A