您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

M9195A/M9195B PXIe Digital Stimulus/Response IVI and MATLAB Instrument Drivers

For a complete list of all instrument drivers from Keysight, please visit www.keysight.com/find/drivers

發佈日期 版本 版本說明
2016-03-23 2.0.2098.0 See description below.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only)

IVI class support: IviDriver 1.0

Version Description:

  • Adds support for the M9195B
  • The Initialize method now allows multiple VISA resource descriptors to be listed in the ResourceName parameter to create a multi-module instrument.
  • The Modules interface has been added to the 2.0 driver to support the ability to query and set the properites of each module in a multi-module instrument. For example, you can query the slot number and temperature of each of several modules.
  • The Trigger interface has been added to support triggers and markers on the M9195A and M9195B. Triggers are input signals to the DSR while markers are output signals from the DSR. Triggers can be used to initiate the execution of PatternSites while markers can be used to trigger other devices.
  • The Sites2 interface has been added to support the Marker0Destination, Marker1Destination, and Marker2Destination properties that are used to generate markers.
  • The PatternSites2 interface has been added to support methods which fetch wide data. Wide data is data wider than the 16 bits supported by the 16 channels of a single module. For 12 modules, the data can be 192 bits wide (12 modules x 16 channels/module).
  • The System2 interface has been added to provide the ability to query the options supported on a module and to query additional module information. The DSR SFP displays this information in its About dialog box.

如何下載

  1. Click the Download button
  2. Choose Run

如何安裝

  • Run the downloaded installer

授權

  • 不需要授權

支援文件

2015-05-21 1.0.10.1 Initial public release

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only)
IVI class support: IviDriver 1.0

如何下載

  1. Click the Download button.
  2. Choose Run

如何安裝

  • Run the downloaded installer

授權

  • 不需要授權

支援文件