Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

N8900 Series Autoraging System DC Power Supply Firmware

Дата выпуска Версия Описание версии
2017-03-17 B.02.05 N8900 series firmware version B.02.05 has added new feature and fixed various bugs.

Как загрузить

  1. Click the Download button.
  2. Save the file to your computer and note the directory where the file is saved. A firmware update installed over the LAN, GPIB, or USB interface is a file with a .upd extension.
  3. Unzip the file to access the .upd file.

Как установить

  • From the utility directory or Start menu, start the utility (FWUpdate.exe). The utility will prompt you for the location of the .upd file. Follow the additional prompts to complete the installation. The update may take several seconds to complete and will reboot the instrument. After the update is complete, exit the utility.
  • It is not necessary to re-calibrate the instrument following a firmware-update; however, the instrument may need to be re-secured if it was unsecured to perform the update.

Лицензии

  • Лицензия не требуется

Сопроводительная документация

Дополнительное ПО/утилиты

Загрузить

Устанавливается на:

Instrument

Операционная система

  • Windows 7
  • Windows XP
  • Windows 2000
  • Windows NT
  • Windows ME

Предварительные условия

  • Download and install Firmware Update Utility software

Поддерживаемые приборы

  • N8920A, N8921A, N8923A, N8924A, N8925A, N8926A, N8928A, N8929A, N8930A, N8931A, N8932A, N8934A, N8935A, N8937A, N8940A, N8941A, N8943A, N8944A, N8945A, N8946A, N8948A, N8949A, N8950A, N8951A, N8952A, N8954A, N8955A, N8957A
2015-09-18 B.02.02 N8900 series firmware version B.02.02 has been rebranded for Keysight. Rear panel Fault and Inhibit functions have been changed to function as in other Keysight products.

Как загрузить

  1. Click the Download button.
  2. Save the file to your computer and note the directory where the file is saved. A firmware update installed over the LAN, GPIB, or USB interface is a file with a .upd extension.
  3. Unzip the file to access the .upd file.

Как установить

  • From the utility directory or Start menu, start the utility (FWUpdate.exe). The utility will prompt you for the location of the .upd file. Follow the additional prompts to complete the installation. The update may take several seconds to complete and will reboot the instrument. After the update is complete, exit the utility.
    It is not necessary to re-calibrate the instrument following a firmware-update; however, the instrument may need to be re-secured if it was unsecured to perform the update.

Лицензии

  • Лицензия не требуется

Сопроводительная документация

Дополнительное ПО/утилиты

Загрузить

Устанавливается на:

Instrument

Операционная система

  • Windows 7
  • Windows XP
  • Windows 2000
  • Windows NT
  • Windows ME

Предварительные условия

  • None

Поддерживаемые приборы

  • N8920A, N8921A, N8923A, N8924A, N8925A, N8926A, N8928A, N8929A, N8930A, N8931A, N8932A, N8934A, N8935A, N8937A, N8940A, N8941A, N8943A, N8944A, N8945A, N8946A, N8948A, N8949A, N8950A, N8951A, N8952A, N8954A, N8955A, N8957A
2014-05-05 A.00.06 N8900 Series firmware version A.00.06 addresses a bug when paralleling units.

Как загрузить

  1. Click the Download button.
  2. Save the file to your computer and note the directory where the file is saved. A firmware update installed over the LAN, GPIB, or USB interface is a file with a .upd extension.
  3. Unzip the file to access the .upd file.

Как установить

  • From the utility directory or Start menu, start the utility (FWUpdate.exe). The utility will prompt you for the location of the .upd file. Follow the additional prompts to complete the installation. The update may take several seconds to complete and will reboot the instrument. After the update is complete, exit the utility.
    It is not necessary to re-calibrate the instrument following a firmware-update; however, the instrument may need to be re-secured if it was unsecured to perform the update.

Лицензии

  • Лицензия не требуется

Сопроводительная документация

Дополнительное ПО/утилиты

Загрузить

Устанавливается на:

Instrument

Операционная система

  • Windows 7
  • Windows XP
  • Windows 2000
  • Windows NT
  • Windows ME

Предварительные условия

  • None

Поддерживаемые приборы

  • N8920A, N8921A, N8923A, N8924A, N8925A, N8926A, N8928A, N8929A, N8930A, N8931A, N8932A, N8934A, N8935A, N8937A, N8940A, N8941A, N8943A, N8944A, N8945A, N8946A, N8948A, N8949A, N8950A, N8951A, N8952A, N8954A, N8955A, N8957A