您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

N8900 Series Autoraging System DC Power Supply Firmware

發佈日期 版本 版本說明
2017-03-17 B.02.05 N8900 series firmware version B.02.05 has added new feature and fixed various bugs.

如何下載

  1. Click the Download button.
  2. Save the file to your computer and note the directory where the file is saved. A firmware update installed over the LAN, GPIB, or USB interface is a file with a .upd extension.
  3. Unzip the file to access the .upd file.

如何安裝

  • From the utility directory or Start menu, start the utility (FWUpdate.exe). The utility will prompt you for the location of the .upd file. Follow the additional prompts to complete the installation. The update may take several seconds to complete and will reboot the instrument. After the update is complete, exit the utility.
  • It is not necessary to re-calibrate the instrument following a firmware-update; however, the instrument may need to be re-secured if it was unsecured to perform the update.

授權

  • 不需要授權

支援文件

外掛軟體/工具程式

下載

安裝於:

Instrument

作業系統

  • Windows 7
  • Windows XP
  • Windows 2000
  • Windows NT
  • Windows ME

必備檔案

  • Download and install Firmware Update Utility software

支援的儀器

  • N8920A, N8921A, N8923A, N8924A, N8925A, N8926A, N8928A, N8929A, N8930A, N8931A, N8932A, N8934A, N8935A, N8937A, N8940A, N8941A, N8943A, N8944A, N8945A, N8946A, N8948A, N8949A, N8950A, N8951A, N8952A, N8954A, N8955A, N8957A
2015-09-18 B.02.02 N8900 系列韌體版本 B.02.02 已更換為是德科技商標。背板上的「錯誤和禁止操作(Fault and Inhibit)」功能已更改為和其他是德科技產品一樣的功能。

如何下載

  1. 點擊下載 按鈕
  2. 將檔案存入電腦中,請記住儲存此壓縮檔的目錄。韌體更新版本可透過 LAN、GPIB 或 USB 介面進行安裝,其副檔名為 .upd
  3. 請解壓縮該檔案以便存取 .upd 檔

如何安裝

  • 在工具程式目錄或 “開始” 功能選單中,啟動該程式(FWUpdate.exe)。它將提示您 .upd 檔的位置。請根據其它提示完成安裝。更新過程將會持續數秒,並要求重啟儀器。更新完畢後,退出該工具程式。
    無需對韌體更新後的儀器重新校驗;但如果儀器在更新過程中呈現解鎖狀態,那麼它需要重新設置安全條件。

授權

  • 不需要授權

支援文件

外掛軟體/工具程式

下載

安裝於:

Instrument

作業系統

  • Windows 7
  • Windows XP
  • Windows 2000
  • Windows NT
  • Windows ME

必備檔案

支援的儀器

  • N8920A, N8921A, N8923A, N8924A, N8925A, N8926A, N8928A, N8929A, N8930A, N8931A, N8932A, N8934A, N8935A, N8937A, N8940A, N8941A, N8943A, N8944A, N8945A, N8946A, N8948A, N8949A, N8950A, N8951A, N8952A, N8954A, N8955A, N8957A
2014-05-05 A.00.06 N8900 Series firmware version A.00.06 addresses a bug when paralleling units.

如何下載

  1. Click the Download button.
  2. Save the file to your computer and note the directory where the file is saved. A firmware update installed over the LAN, GPIB, or USB interface is a file with a .upd extension.
  3. Unzip the file to access the .upd file.

如何安裝

  • From the utility directory or Start menu, start the utility (FWUpdate.exe). The utility will prompt you for the location of the .upd file. Follow the additional prompts to complete the installation. The update may take several seconds to complete and will reboot the instrument. After the update is complete, exit the utility.
    It is not necessary to re-calibrate the instrument following a firmware-update; however, the instrument may need to be re-secured if it was unsecured to perform the update.

授權

  • 不需要授權

支援文件

外掛軟體/工具程式

下載

安裝於:

Instrument

作業系統

  • Windows 7
  • Windows XP
  • Windows 2000
  • Windows NT
  • Windows ME

必備檔案

  • None

支援的儀器

  • N8920A, N8921A, N8923A, N8924A, N8925A, N8926A, N8928A, N8929A, N8930A, N8931A, N8932A, N8934A, N8935A, N8937A, N8940A, N8941A, N8943A, N8944A, N8945A, N8946A, N8948A, N8949A, N8950A, N8951A, N8952A, N8954A, N8955A, N8957A