Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discuter avec un expert

VISA Shared Components downloads

The VISA Shared Components is a required component for the IO Libraries Suite to operate correctly. The correct version of the VISA Shared Components is installed by the IO Libraries Suite, so users don't typically need to worry about installing this package.

However, if you need to repair, or install an older version of the VISA Shared Components you can download it here.

Date de mise en circulation Version Description de la version
2013-12-01 1.6 Updated the USB-TMC kernel driver to address issues with USB 3.0. Added support for the new VISA COM interface IRegister64_2. Changed the downloadable installer to be a self-extracting EXE rather than the raw MSI.

Comment télécharger

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

Comment installer

  • Run the downloaded installer

Autorisation d'exploitation

  • Ne requiert aucune licence

Document d'appui

Logiciels additionels/utilités

Téléchargez

S'installe sur:

PC

Système d'exploitation

  • Windows 8
  • Windows 7
  • Windows Vista
  • Windows XP

Préalables

  • No prerequisites.