您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

M9393A PXIe Performance Vector Signal Analyzer Instrument Drivers

For a complete list of all instrument drivers from Keysight, please visit www.keysight.com/find/drivers

發佈日期 版本 版本說明
2017-05-25 2.1.910.2 See description above.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only), LabVIEW (32-bit/64-bit)

IVI class support: IviDriver 1.0

LabVIEW driver version: 2.0.3

Version Description:

  • When the M9393A driver is initialized with “ExternalDigitizer=true” or “ExternalDigitizer=1” in the option string, M9214A IF Digitizer is no longer required in the PXI chassis.
  • A new M9393 wideband IF hardware extension for the 89600 VSA has been added that allows a M9393A to be paired with a M9203A digitizer to obtain measurement bandwidth up to 1 GHz.
  • New FPGA bits with improved stability.

如何下載

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安裝

  • Run the downloaded installer.

授權

  • 不需要授權

支援文件

2016-09-04 2.1.875.1 See description below.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only), LabVIEW (32-bit/64-bit)

IVI class support: IviDriver 1.0

LabVIEW driver version: 2.0.3

Version Description:

  • Enhanced support for list mode with external attenuator configuration.
  • Corrected external attenuator module identification.
  • Corrected selection of external attenuator module in simulation mode.
  • Corrected field alignment backwards compatibility with 1.x factory calibration data.
  • Corrected resource locking for the M9300 Reference module.

如何下載

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安裝

  • Run the downloaded installer.

授權

  • 不需要授權

支援文件

2016-03-31 2.1.855.0 See description below.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only), LabVIEW (32-bit/64-bit)

IVI class support: IviDriver 1.0

LabVIEW driver version: 2.0.3

Version Description :

  • Added property, RF3.Attenuator, to select RF attenuator type used for certain hardware configurations.
  • Added property, RF3.AttenuatorMode, to control the RF input signal path in front of the mixer.
  • Added interface, FFTAcquisition2.NoiseCorrection, with properties Enabled and Mode to support noise correction in FFT acquisition mode.
  • M9300A-Carrier FPGA 1.0.4.0 available – Optional, not currently required for any new software features.

如何下載

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安裝

  • Run the downloaded installer.

授權

  • 不需要授權

支援文件

2016-01-29 2.0.225.1 See description below.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only), LabVIEW (32-bit/64-bit)

IVI class support: IviDriver 1.0

LabVIEW driver version: 2.0.3

Version Description :

  • Enhanced self-tests and corrections for installed hardware options.
  • Enhanced support for external applications software.
  • Increased IF frequency range to [200 MHz, 800 MHz] for external wideband digitizers.

如何下載

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安裝

  • Run the downloaded installer.

授權

  • 不需要授權

支援文件

2015-11-06 2.0.200.0 See description below.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only), LabVIEW (32-bit/64-bit)

IVI class support: IviDriver 1.0

LabVIEW driver version: 1.1.2

Version Description :

  • Support for extended frequency range (3.6 GHz - 50 GHz) using option M9365A-FRX. Use of M9169E Programmable Attenuator is recommended for range control, automated field alignments, and self test.
  • Support for wideband IF (up to 800 MHz) using option M9365A-WB1 and use of an external wideband digitizer, such as M9202A or M9703A.
  • Limited (setup) support for data streaming using the M9202A wideband digitizer. All streaming controls are available from the M9392A VSA Soft Front Panel and IVI interfaces.
  • Support for peer-to-peer IQ data transfer from the M9214A Digitizer module to another module that supports peer-to-peer data transfer, such as the M9451A module, using the PeertoPeerPort IVI interface.
  • Enhanced self-tests for extended frequency ranges with or without the M9169E Step Attenuator.
  • 89600: Power Spectrum speed improvements

如何下載

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安裝

  • Run the downloaded installer.

授權

  • 不需要授權

支援文件

2015-09-19 1.2.1019.1 See description below.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only), LabVIEW (32-bit/64-bit)

IVI class support: IviDriver 1.0

LabVIEW driver version: 1.1.2

Version Description :

Various defects fixed:

  • Corrected frequency scaling for soft front panel FFT Acquisition mode
  • Increased maximum value for soft front panel IQ averaging period to match IVI maximum
  • Fixed intermittent glitch on narrowband time trace after using FFT Acquisition mode

     

如何下載

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安裝

  • Run the downloaded installer.

授權

  • 不需要授權

支援文件

2015-05-23 1.2.1016.0 See description below.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only), LabVIEW (32-bit/64-bit)

IVI class support: IviDriver 1.0

LabVIEW driver version: 1.1.2

Version Description :

Added Support for M9415A Peer To Peer operation. Not supported via IVI.
Added Support for M9415A Noise Correction in FFT Acquisition Mode. Not supported via IVI.
 

Various defects fixed:
WIT 385288 – LO Feedthrough causes IF Overloads when using Noise Corrections
WIT 391319 – Interaction with M90XA prevents newer M90XA versions from running

 

如何下載

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安裝

  • Run the downloaded installer.

授權

  • 不需要授權

支援文件

2015-03-20 1.1.522.2 Enhancement to field calibration that improves expected input level accuracy, Fixture Loss Enabled is now set to False on Reset

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only), LabVIEW (32-bit/64-bit)

IVI class support: IviDriver 1.0

LabVIEW driver version: 1.1.2

如何下載

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.
     

如何安裝

  • Run the downloaded installer.

授權

  • 不需要授權

支援文件

2015-02-13 1.1.518.1 See description below.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only), LabVIEW (32-bit/64-bit)

IVI class support: IviDriver 1.0

LabVIEW driver version: 1.1.2

Version description:

  • 89600: allow driver sharing using M9000 resource manager for multi-channel configurations
  • Various defects fixed:
    • WIT 353338 – Issue starting system if locale uses comma as decimal separator
    • WIT 357918 – LO Nulling intermittently fails on some systems
    • WIT 369709 – Issue with field calibration resulting in ~0.2 dB flatness error on some units
    • WIT 335725 – 89600: error reported when IF Dither enabled and Span/RBW ratio too large
    • WIT 353408 – 89600: error reported when switching between IF Mag & External Trigger in Sequenced Mode
    • WIT 353905 – 89600: minimum gate length limited to 100 ns in zero span
    • WIT 355118 – 89600: added VBW limiting in zero span
    • WIT 356920 – 89600: channel filter was not set correctly for non-power spectrum measurements
    • WIT 359033 – 89600: allow higher Span to RBW ratio based on physical memory available 

如何下載

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安裝

  • Run the downloaded installer.

授權

  • 不需要授權

支援文件

2014-09-25 1.1.240.0 See description below.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only), LabVIEW (32-bit/64-bit)

IVI class support: IviDriver 1.0

LabVIEW driver version: 1.1.2

Version description:

  • Added LabVIEW driver for M9393A
  • Added IF Dither mode for Stepped Spectrum
    • See IAgM9393Ex2.SteppedSpectrumAcquisition2.IFDither.*
  • Added multi-channel synchronization
    • See IAgM9393.MultiChannelSync.*
  • Defect WIT 337258: 89600 - Overlap Percentage error with Gate Trigger and Power Spectrum
  • Defect WIT 339914: Comprehensive alignment failed if initial instrument state is Stepped Spectrum and conversion is image protect
  • Documentation updates
     

如何下載

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安裝

  • Run the downloaded installer.

授權

  • 不需要授權

支援文件

2014-08-12 1.0.80.1 Defect fixes: Alignments fail if conversion mode is not set to Auto, or multiple instances of M9393 in same process. Corrected trigger qualification of wideband burst trigger for IVI/89600. Several defects using 89600 software. See readme for details

如何下載

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安裝

  • Run the downloaded installer.

授權

  • 不需要授權

支援文件

2014-08-05 1.0.70.0 Initial release.

如何下載

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安裝

  • Run the downloaded installer.

授權

  • 不需要授權

支援文件