An update may take up to 60 minutes to complete depending on the type of components requiring an update. During this time, instrument modules installed in the chassis are deactivated to the ATCA service state to reduce power consumption and are unavailable for applications. The chassis fan speed may change during the update as well. Following the update, cycle chassis power to complete the installation.

Keysight recommends using the most current version, which includes the most up-to-date bug fixes and security patches available.
Release Date Version Version Description
2014-08-04 2.3.11 If you are using a remote PC that has an Intel Haswell based processor, then you will need to use this firmware update.
Release Date Version
2014-08-04 2.3.11
Version Description
If you are using a remote PC that has an Intel Haswell based processor, then you will need to use this firmware update.

How to Download

  1. Click Download button
  2. Save .zip file to host computer (c:/tmp)
  3. Unzip the package to your PC

How to Install

  1. To open the M9521A Chassis Soft Front Panel, from Windows click:
  2. Start > All Programs > Agilent > AXIe Chassis (M9521) > AXIeC SFP
  3. From the SFP, click Utilities > Update Firmware... and follow the instructions in the dialog boxes and the application help.

Licensing

  • Does Not Require a License

Installs on: Instrument

Operating System

  • Windows 7 (SP1)
  • Windows 8.1

Prerequisites

  • IO Libraries 16.3 or later

Supported Instruments

  • M9514A

How to Download

  1. Click Download button
  2. Save .zip file to host computer (c:/tmp)
  3. Unzip the package to your PC

How to Install

  1. To open the M9521A Chassis Soft Front Panel, from Windows click:
  2. Start > All Programs > Agilent > AXIe Chassis (M9521) > AXIeC SFP
  3. From the SFP, click Utilities > Update Firmware... and follow the instructions in the dialog boxes and the application help.

Licensing

  • Does Not Require a License

Installs on: Instrument

Operating System

  • Windows 7 (SP1)
  • Windows 8.1

Prerequisites

  • IO Libraries 16.3 or later

Supported Instruments

  • M9514A
SHOW MORE