Use the DOCSIS 3.1 configuration wizard to create the OFDM setup files for 89600 VSA custom OFDM (Option BHF) based on the downstream and upstream configurations.

These files are not available in the 89600 VSA software DVD or webhelp file.

キーサイトは、最新のバグ修正とセキュリティパッチを含む、利用可能な最新バージョンを使用することをお勧めします。
リリース バージョン 内容
2015-10-06 1.4.6.0 New feature: Modified menus of DOCSIS 3.1 upstream wizard with upper/lower guard subcarriers, additional setup file creation with SpanOptimized checkbox, and some defect fixes.
リリース バージョン
2015-10-06 1.4.6.0
Version Description
New feature: Modified menus of DOCSIS 3.1 upstream wizard with upper/lower guard subcarriers, additional setup file creation with SpanOptimized checkbox, and some defect fixes.

ダウンロード方法

  • Click on the Download button
  • Select Save
  • Extract the files from the zip file to a folder on your hard drive
  • Double-click on Setup-DOCSIS31-Wizard.msi to install the wizard

インストール方法

  • See Supporting Documentation

ライセンス

  • Does Not Require a License

Installs on: PC

OS

  • Windows 8 Professional
  • Windows 8 Enterprise
  • Windows 7 Professional
  • Windows 7 Enterprise
  • Windows 7 Ultimate

ダウンロード方法

  • Click on the Download button
  • Select Save
  • Extract the files from the zip file to a folder on your hard drive
  • Double-click on Setup-DOCSIS31-Wizard.msi to install the wizard

インストール方法

  • See Supporting Documentation

ライセンス

  • Does Not Require a License

Installs on: PC

OS

  • Windows 8 Professional
  • Windows 8 Enterprise
  • Windows 7 Professional
  • Windows 7 Enterprise
  • Windows 7 Ultimate

前提知識

  • 89600 VSA v18.5 or later to be installed, licensed with Options 200, 300 and BHF (required for the wizard to create Custom OFDM setup files for DOCSIS 3.1 formats)

ダウンロード方法

  • Click on the Download button
  • Select Save
  • Extract the files from the zip file to a folder on your hard drive
  • Double-click on Setup-DOCSIS31-Wizard.msi to install the wizard

インストール方法

  • See Supporting Documentation

ライセンス

  • Does Not Require a License

Installs on: PC

OS

  • Windows 8 Professional
  • Windows 8 Enterprise
  • Windows 7 Professional
  • Windows 7 Enterprise
  • Windows 7 Ultimate

前提知識

  • 89600 VSA v18.5 or later to be installed, licensed with Options 200, 300 and BHF (required for the wizard to create Custom OFDM setup files for DOCSIS 3.1 formats)

ダウンロード方法

  • Click on the Download­ button
  • Select Save
  • Extract the files from the zip file to a folder on your hard drive
  • Double-click on DOCSIS31.exe to run the wizard

インストール方法

  • See Supporting Documentation

ライセンス

  • Does Not Require a License

Installs on: PC

OS

  • Windows 8 Professional
  • Windows 8 Enterprise
  • Windows 7 Professional
  • Windows 7 Enterprise
  • Windows 7 Ultimate

前提知識

  • 89600 VSA v18 or later to be installed, licensed with Options 200, 300 and BHF (required­for the­wizard to create Custom OFDM setup files for DOCSIS 3.1 formats)

対象測定器

  • N9070A Wideband Signal Analysis Solutions
SHOW MORE