Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discuter avec un expert

E6607x EXT Wireless Communications Test Set IVI and MATLAB Instrument Drivers

For a complete list of all instrument drivers from Keysight, please visit www.keysight.com/find/drivers

This driver download installs the IVI-C, IVI-COM, and MATLAB driver components.

Keysight IVI drivers also require that Keysight IO Libraries Suite be installed. To get the latest release of the IO Libraries Suite, go to www.keysight.com/find/iosuite

Current Version Details
Version 1.1.2.0
Models Supported E6607A, E6607B, E6607C
Driver Types and Version IVI-C (32-bit/64-bit)
IVI-COM (32-bit/64-bit)
MATLAB (32-bit)
IVI Classes Supported IviDriver 1.0
Minimum IVI Shared Components Version  2.2.1.0 
Date de mise en circulation Version Description de la version
2013-11-21 1.1.2.0 Added support for E6607C which includes the MultiportAdapter and System2 interfaces and the MultiportAdapterCorrection repeated capability.

Comment télécharger

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

Comment installer

  • Run the downloaded installer.

Autorisation d'exploitation

  • Ne requiert aucune licence

Document d'appui