이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

고급 파워 시스템 N6900 & N7900 펌웨어

릴리스 날짜 버젼 버전 설명
2019-03-27 A.02.01.1256 Enhancement

다운로드 방법

  1. Click the Download button.
  2. Save the file to your computer and note the directory where the file is saved. A firmware update installed over the LAN, GPIB, or USB interface is a file with a .upd extension.
  3. Unzip the file to access the .upd file.

설치 방법

  • From the utility directory or Start menu, start the utility (FWUpdate.exe). The utility will prompt you for the location of the .upd file. Follow the additional prompts to complete the installation. The update may take several seconds to complete and will reboot the instrument. After the update is complete, exit the utility.
    It is not necessary to re-calibrate the instrument following a firmware-update; however, the instrument may need to be re-secured if it was unsecured to perform the update.
     

라이센스

  • 라이센스 필요 없음

지원 문서

부가 소프트웨어 / 유틸리티

다운로드

설치 위치:

Instrument

운영 체제

  • Windows 7
  • Windows XP

사전 조건

  • Firmware Update Utility

지원되는 계측기

  • N6950A, N6951A, N6952A, N6953A, N6954A, N6970A, N6971A, N6972A, N6973A, N6974A, N6976A, N6977A, N7950A, N7951A, N7952A, N7953A, N7954A, N7970A, N7972A, N7973A, N7974A, N7976A, N7977A