Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Advanced Power System N6900 & N7900 Firmware

Which version of the firmware is right for my products?
Check the current firmware revision
Go to Menu -> System-> About (Firmware version)
A.xx.xx.xxxx - use last applicable firmware revision A at Previous Version Tab
B.xx.xx.xxxx - use firmware revision B.02.01.1256 and above.

Note: A revision firmware is for old(P500) processor instrument, and is not compatible with new processor(P600) instrument
B revision firmware is for new processor instrument, and is not compatible with old processor instrument

Release Date Version Version Description
2019-10-16 B.02.01.1256 Initial Release for New Processor (P600)

How to Download

  1. Click the Download button.
  2. Save the file to your computer and note the directory where the file is saved. A firmware update installed over the LAN, GPIB, or USB interface is a file with a .upd extension.
  3. Unzip the file to access the .upd file.

How to Install

  • From the utility directory or Start menu, start the utility (FWUpdate.exe). The utility will prompt you for the location of the .upd file. Follow the additional prompts to complete the installation. The update may take several seconds to complete and will reboot the instrument. After the update is complete, exit the utility.
    It is not necessary to re-calibrate the instrument following a firmware-update; however, the instrument may need to be re-secured if it was unsecured to perform the update.
     

Licensing

  • Does Not Require a License

Supporting Documentation

Add-On Software / Utilities

Download

Installs on:

Instrument

Operating System

  • Windows 7
  • Windows XP

Prerequisites

  • Firmware Update Utility

Supported Instruments

  • N6950A, N6951A, N6952A, N6953A, N6954A, N6970A, N6971A, N6972A, N6973A, N6974A, N6976A, N6977A, N7950A, N7951A, N7952A, N7953A, N7954A, N7970A, N7972A, N7973A, N7974A, N7976A, N7977A