Keysight empfiehlt die Verwendung der aktuellen Version, die die neuesten verfügbaren Fehlerbehebungen und Sicherheitspatches enthält.
Veröffentlichungsdatum Version Versionsbeschreibung
2017-03-01 3.09-3.00-3.06 U3606B Firmware Upgrade, Revision 3.09-3.00-3.06.
Veröffentlichungsdatum Version
2017-03-01 3.09-3.00-3.06
Version Description
U3606B Firmware Upgrade, Revision 3.09-3.00-3.06.

How to Download

  • 1. Click the Download button
    2. Save the file to your PC or desktop

Lizenzierung

  • Does Not Require a License

Supporting Documentation

Installs on: Instrument

Operating System

  • Windows 7
  • Windows XP SP3
  • Windows 2000

Voraussetzungen

  • System Requirements:
    Processor: 100 MHz Pentium II or higher required, 800 MHz recommended.
    Required Software:
    .NET Framework 2.0 or above.
    Windows Installer 3.0. Windows Installer 3.1 or later is recommended.
    Keysight IO Libraries Suit 14.0 and above

Supported Instruments

  • U3606B

How to Download

  • 1. Click the Download button
    2. Save the file to your PC or desktop
    ­

Lizenzierung

  • Does Not Require a License

Supporting Documentation

Installs on: Instrument

Operating System

  • Windows 7
  • Windows XP SP3
  • Windows 2000

Voraussetzungen

  • System Requirements:
    Processor: 100 MHz Pentium II or higher required, 800 MHz recommended.
    Required Software:
    .NET Framework 2.0 or above.
    Windows Installer 3.0. Windows Installer 3.1 or later is recommended.
    Keysight IO Libraries Suit 14.0 and above
    ­

Supported Instruments

  • U3606B

How to Download

  • 1. Click the Download button
    2. Save the file to your PC or desktop
     

Lizenzierung

  • Does Not Require a License

Supporting Documentation

Installs on: Instrument

Operating System

  • Windows 7
  • Windows XP SP3
  • Windows 2000

Voraussetzungen

  • System Requirements:
    Processor: 100 MHz Pentium II or higher required, 800 MHz recommended.
    Required Software:
    .NET Framework 2.0 or above.
    Windows Installer 3.0. Windows Installer 3.1 or later is recommended.
    Agilent IO Libraries Suit 14.0 and above

Supported Instruments

  • U3606B

How to Download

  • 1. Click the Download button
    2. Save the file to your PC or desktop

How to Install

  • Installing the software:

  • 1. Unzip the zip file to a folder.
    2. Select setup.exe to start installation.

  • Updating the firmware:

  • 1. On U3606B: Access to Utility menu and select

  • Lizenzierung

    • Does Not Require a License

    Supporting Documentation

    Installs on: Instrument

    Operating System

    • Windows 7
    • Windows XP SP3
    • Windows 2000

    Voraussetzungen

    • System Requirements:
      Processor: 100 MHz Pentium II or higher required, 800 MHz recommended.
      Required Software:
      .NET Framework 2.0 or above.
      Windows Installer 3.0. Windows Installer 3.1 or later is recommended.
      Agilent IO Libraries Suit 14.0 and above

    Supported Instruments

    • U3606B

    How to Download

    • 1. Click the Download button
      2. Save the file to your PC or desktop
       

    How to Install

    • Installing the software:
      1. Unzip the zip file to a folder.
      2. Double click the setup.exe file to start installing.
      3. Follow the instructions to install the program.

    • Updating the firmware:
      1. On the U3606B: Select "U-tMC" as the remote interface connection.
      2. Connect the U3606B to the PC using the USB cable.
      3. Ensure that you have Agilent IO Libraries Suite installed but do not enable it (exit it at this stage).
      4. Go to Start >All Programs >Agilent > U3606B Firmware Update (Version 1.01-1.09-1.05) and start the firmware update.
      5. Do not power off the U3606B during the update process. If a "Power cycle the U3606B" message box appears, power cycle the unit and resume the firmware update.
      6. Reboot the unit after the firmware upgrade is completed.
       

    Lizenzierung

    • Does Not Require a License

    Supporting Documentation

    Installs on: Instrument

    Operating System

    • Windows XP SP3
    • Windows 2000

    Voraussetzungen

    • System Requirements
      Processor: 100 MHz Pentium II or higher required, 800 MHz recommended.

      Supported Operating Systems:
      Windows 2000 Service Pack 3 or latest;
      Windows XP Service Pack 2 or latest

    • Required Software:
      .NET Framework 2.0 or above.
      Windows Installer 3.0. Windows Installer 3.1 or later is recommended.
      Agilent IO Libraries Suit 14.0 and above

    • Disk Space Requirements:
      2.86MB
       

    Supported Instruments

    • U3606B
    SHOW MORE