이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

B1500A/B1505A Utility : IC-CAP MDM File Converter for B1500A/B1505A EasyEXPERT

B1500A/B1505A Utility : IC-CAP MDM File Converter for B1500A/B1505A/EasyEXPERT

MDM File Converter A.01.03

릴리스 날짜 버젼 버전 설명
2014-01-14 A.01.03 A.01.03.2014.0108

다운로드 방법

  • Click the "Download" button.

설치 방법

  • 1. Expand the contents of the downloaded file into a working folder as follows.
        a) Go to the folder where the downloaded file is saved and open the folder.
        b) Place the pointer on the downloaded file and click the mouse right button
            and select "Extract All...".
        NOTE: If any unzip tool is installed, the above may not work.
                  In this case, follow the instruction of the tool.
                  Below is an example for the tool "winzip".
                  - Firstly double-click the donloaded file, then click "unzip" in the
                    menu bar. Then specify the folder and click "unzip".
    2. Insert the Desktop EasyEXPERT software CD-ROM into the CD-ROM drive.
    3. Double click the index.html file in the CD-ROM.
    4. Click "Install MDM File Converter" icon and follow the instructions of the setup wizard.
    5. Wait for installation to complete, and remove the CD-ROM from the CD-ROM drive.
     

라이센스

  • 라이센스 필요 없음

지원 문서

다운로드

설치 위치:

PC

운영 체제

  • Windows 7
  • Windows Vista
  • Windows XP SP3
  • Windows XP SP2

사전 조건

  • See Readme file.

지원되는 계측기

  • B1500A, B1505A